Hi all:
I want to test the bt mesh LPN, so I have configured the mesh light ctl server as a low power node, but the app can't find the Provision Device.
I want to know if the way to adding the network of the LPN is the same as the relay node or friend node.
the testing platform is CYW20735
thanks!
mandy
Solved! Go to Solution.
Hi,
Low power node may go to sleep after a period of time, and when it is in sleep you cannot see the mesh unnprovisioned beacons.
So please press the reset button on the board and then scan for the unprovisioned beacons from the mobile.
Thanks.
-Dheeraj
Hi,
Low power node may go to sleep after a period of time, and when it is in sleep you cannot see the mesh unnprovisioned beacons.
So please press the reset button on the board and then scan for the unprovisioned beacons from the mobile.
Thanks.
-Dheeraj
Hi DheerajP_41:
I have read the SDK code carefully. I find out a low power node struct:
typedef PACKED struct
{
uint8_t rssi_factor; /**< The contribution of the RSSI measured by the Friend node used in Friend Offer Delay calculations.Must be <= 3. RSSIFactor = 1 + (rssi_factor * 0.5) */
uint8_t receive_window_factor; /**< The contribution of the supported Receive Window used in Friend Offer Delay calculations.Must be <= 3. ReceiveWindowFactor = 1 + (receive_window_factor * 0.5) */
uint8_t min_cache_size_log; /**< The minimum number of messages that the Friend node can store in its Friend Cache.Must be >= 1 and <= 7. MinCacheSizeLog = 2 * * min_cache_size_log */
uint8_t receive_delay; /**< Receive delay in 1 ms units to be requested by the Low Power node. It should be >= 0x0a */
uint32_t poll_timeout; /**< Poll timeout in 100ms units to be requested by the Low Power node. It should be between 0x00000a and 0x34bbff */
uint8_t startup_unprovisioned_adv_to; /**< Interval in seconds of the advertisments of unprovisioned beacon and service on startup. Value 0 means default 30 seconds. */
} wiced_bt_mesh_core_config_low_power_t;
the member variable : tartup_unprovisioned_adv_to is not been initialized, when I have initialized it to 0x7F, I can find the unprovisioned device by phone
I don't know the detail meaning of startup_unprovisioned_adv_to, Can you explain it to me ?
thank you !
Hi mandy wu,
As described in the comment, it is the period of time the LPN node can advertise unprovisioned beacons.
By default it is configured as 0 which is equal to 30 seconds. If you configure it to 127, then it means the advertisement will go off after 127 seconds.
After the timeout you will be able to see below print in the teraterm (PUART log) which indicate that device entered in the sleep mode.
mesh_state_changed_cb:LPN_SLEEP: timeout:-1
Using the default configuration of the app, can you try your experiment in a low noisy environment? I recommend you to use Windows meshClient application for this test?
I doubt that this 30sec is not enough for your phone to detect the adv of unprovisioned mesh device.It can occur due to more noisy environment (more BT, WiFi devices in the room) or capability of test phone to detect wireless activity is less.
Thanks,
-Dheeraj