Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

mawu_4270096
Level 5
5 sign-ins First like received First like given
Level 5

Hi   all:

       I  am very confused  that  why the CTL Server model includes the  Level server and  lightness server,  As I know, the  level  server model have  realized the same functions with lightness server,  I  don't  know what are the differences between Level server model and lightness server model, who  can tell me?

#define WICED_BT_MESH_MODEL_LIGHT_CTL_SERVER \
    { MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_GENERIC_DEFTT_SRV, wiced_bt_mesh_model_default_transition_time_server_message_handler, NULL, NULL }, \
    { MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_SCENE_SRV, wiced_bt_mesh_model_scene_server_message_handler, NULL, NULL }, \
    { MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_SCENE_SETUP_SRV, wiced_bt_mesh_model_scene_setup_server_message_handler, NULL, NULL }, \
    { MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_SCHEDULER_SRV, wiced_bt_mesh_model_scheduler_server_message_handler, NULL, NULL }, \
    { MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_SCHEDULER_SETUP_SRV, wiced_bt_mesh_model_scheduler_setup_server_message_handler, NULL, NULL }, \
    { MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_TIME_SRV, wiced_bt_mesh_model_time_server_message_handler, NULL, NULL }, \
    { MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_TIME_SETUP_SRV, wiced_bt_mesh_model_time_setup_server_message_handler, NULL, NULL }, \
    { MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_GENERIC_ONOFF_SRV, wiced_bt_mesh_model_onoff_server_message_handler, NULL, NULL }, \
    { MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_GENERIC_POWER_ONOFF_SRV, wiced_bt_mesh_model_power_onoff_server_message_handler, NULL, NULL }, \
    { MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_GENERIC_POWER_ONOFF_SETUP_SRV, wiced_bt_mesh_model_power_onoff_setup_server_message_handler, NULL, NULL }, \
    { MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_GENERIC_LEVEL_SRV, wiced_bt_mesh_model_level_server_message_handler, NULL, NULL }, \
    { MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_LIGHT_LIGHTNESS_SRV, wiced_bt_mesh_model_light_lightness_server_message_handler, NULL, NULL }, \
    { MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_LIGHT_LIGHTNESS_SETUP_SRV,  wiced_bt_mesh_model_light_lightness_setup_server_message_handler, NULL, NULL }, \
    { MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_LIGHT_CTL_SRV, wiced_bt_mesh_model_light_ctl_server_message_handler, wiced_bt_mesh_model_light_ctl_server_scene_store_handler, wiced_bt_mesh_model_light_ctl_server_scene_recall_handler }, \
    { MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_LIGHT_CTL_SETUP_SRV, wiced_bt_mesh_model_light_ctl_setup_server_message_handler, NULL, NULL  }

0 Likes
1 Solution
DheerajPK_41
Moderator
Moderator 750 replies posted 500 likes received 500 replies posted
Moderator

Hi,

Macros such as WICED_BT_MESH_MODEL_LIGHT_CTL_SERVER can be used to instantiate mesh models on a given element. Based on the device definition the mesh core creates a device composition data that can be read by the the provisioner.  Here, each model consists of the model definition itself (company ID and model ID) and callback function which is executed by the Mesh Core library on receiving a mesh message.

Eg:

{ MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_GENERIC_LEVEL_SRV, wiced_bt_mesh_model_level_server_message_handler, NULL, NULL },

{ MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_LIGHT_LIGHTNESS_SRV, wiced_bt_mesh_model_light_lightness_server_message_handler, NULL, NULL }

Here, wiced_bt_mesh_model_level_server_message_handler will be called when core receives a valid message for Level Model,and wiced_bt_mesh_model_light_lightness_server_message_handler will be called when core receives a valid message for Light Lightness Server model. These call back functions are defined in the mesh libraries.

Below structure defines configuration data of a model. Please see wiced_bt_mesh_cfg.h.

typedef PACKED struct

{

    uint16_t  company_id;               /**< Company ID of the model. It is 0 for SIG models */

    uint16_t  model_id;                 /**< Model ID */

    void      *p_message_handler;       /**< message handler for this model */

    void      *p_scene_store_handler;   /**< function to call to store the scene contents */

    void      *p_scene_recall_handler;  /**< function to call to recall the scene contents */

} wiced_bt_mesh_core_config_model_t;

Thanks,

-Dheeraj

View solution in original post

1 Reply
DheerajPK_41
Moderator
Moderator 750 replies posted 500 likes received 500 replies posted
Moderator

Hi,

Macros such as WICED_BT_MESH_MODEL_LIGHT_CTL_SERVER can be used to instantiate mesh models on a given element. Based on the device definition the mesh core creates a device composition data that can be read by the the provisioner.  Here, each model consists of the model definition itself (company ID and model ID) and callback function which is executed by the Mesh Core library on receiving a mesh message.

Eg:

{ MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_GENERIC_LEVEL_SRV, wiced_bt_mesh_model_level_server_message_handler, NULL, NULL },

{ MESH_COMPANY_ID_BT_SIG, WICED_BT_MESH_CORE_MODEL_ID_LIGHT_LIGHTNESS_SRV, wiced_bt_mesh_model_light_lightness_server_message_handler, NULL, NULL }

Here, wiced_bt_mesh_model_level_server_message_handler will be called when core receives a valid message for Level Model,and wiced_bt_mesh_model_light_lightness_server_message_handler will be called when core receives a valid message for Light Lightness Server model. These call back functions are defined in the mesh libraries.

Below structure defines configuration data of a model. Please see wiced_bt_mesh_cfg.h.

typedef PACKED struct

{

    uint16_t  company_id;               /**< Company ID of the model. It is 0 for SIG models */

    uint16_t  model_id;                 /**< Model ID */

    void      *p_message_handler;       /**< message handler for this model */

    void      *p_scene_store_handler;   /**< function to call to store the scene contents */

    void      *p_scene_recall_handler;  /**< function to call to recall the scene contents */

} wiced_bt_mesh_core_config_model_t;

Thanks,

-Dheeraj