Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
mawu_4270096
Level 5
Level 5
50 replies posted 25 replies posted 10 replies posted

Hi  all:

     I  have not found the API to notify the status changes of a node to the app, this question  will cause the  app status is out of  sync with device status

    the status is light  lightness, color temperature value, and so on !

thanks!

mandy

0 Likes
1 Solution

Is the question about the lightness and color temperature or a step motor :-). For the Light CTL model, See apps/snip/mesh/mesh_light_ctl_server.c, the call is

    wiced_bt_mesh_model_light_ctl_server_state_changed(...);

Note that your device needs to be configured for Publication to send unsolicited messages.

For the step motor, unfortunately there is no standard model. You can use Vendor Specific model and send whatever messages you need.

Note that you should be pretty careful with mesh messages, because the bandwidth is very limited. If your application does not need to send messages, do not send them. If phone UI does not require update more than once per second, configure your step motor to publish data once per second. You can also configure for publication when entering the screen and unconfigure when exiting the screen.

View solution in original post

3 Replies