Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Studio Bluetooth Forum Discussions

WaZh_4062111
Studio Bluetooth
I am using the EZ-Serial firmware for this module and I'm having an issue where pairing connects to the BLE instead of BT-Classic. Is there anyway to ... Show More
StBa_721356
Studio Bluetooth
When using wiced_bt_ble_scan() we see that after restarting it with another call to wiced_bt_ble_scan() we do get advert data from peripherals which d... Show More
RSK_2736041
Studio Bluetooth
We are using SPP profile and I am not sure how and where can I add the BT_LOCAL_NAME + WICED_DEVICE_ADDRESS.I looked at the other post about MAC Addre... Show More
mawu_4270096
Studio Bluetooth
Hi :  I want to know if there is any sample code to use the CYW20735 SPI , if I can do the SPI  communication on the CYW920735q60EVB-01.   it  seems t... Show More
Euso_4258576
Studio Bluetooth
Hello, I have been currently encountering a FW download fail on CYBT-353027.(EVB)Belows are what I had tried so for.1. Using Cypress WICED Studio 6.2I... Show More
TaMi_1708256
Studio Bluetooth
Please tell me the impedance(ohm) when Signal of CYW20706 is set to output.Especially I want to know the value of the following signal.SPI2_MISO_I2S_S... Show More
KeSh_4337371
Studio Bluetooth

Is there any way to convert hcd to bin or hex ?

Eric_wang
Studio Bluetooth

请问在安卓平台上,20706工作在HCI模式,是否可以实现同时连接蓝牙HID手柄,并同时支持连接蓝牙耳机播放音乐,谢谢!

mawu_4270096
Studio Bluetooth
Hi:    according to the documents ,I have  realized  the bluetooth mesh scene,but I have some doubts  1.  as we know,the CYW20735 have not  On-chip f... Show More
MaLu_4280191
Studio Bluetooth

How do I enable multiple simultaneous SPP sessions on the 20719?

Forum Information

Studio Bluetooth

Discussion forum regarding WICED Studio Bluetooth topics.