Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Studio Bluetooth Forum Discussions

ryli_4531716
Studio Bluetooth
Hi, after mount a auth ic in CYW20706evb U4 postition and open SW7 pos 6-8 switch to on, before using iap2 apis, how to ensure this i2c connection is ... Show More
StN__1917156
Studio Bluetooth
Cysmart mobile v1.2 for Android has an option in settings 'Initiate Pairing after Connection' and according to manual:"1.6.1.2.3 ...the CySmart app wi... Show More
StN__1917156
Studio Bluetooth
What function(s) from WICED SDK could use to convert Resolvable Private Address to Identity Address?Let say I’m trying to compare last saved in the NV... Show More
JoOr_4004241
Studio Bluetooth
I am using a CYBT-423028-EVAL board with CYBT-423028-02/CYW20719 dual mode Bluetooth BR/EDR + BLE module. I'm using WICED Studio 6.2 for software deve... Show More
YoJa_3107936
Studio Bluetooth
HiWhen checking PCB layout, two numbers are unknown,Could you explain which is right?1. Pad PitchDepending on your Datasheet, the PadPitch is 1.22mm.I... Show More
siaa_4420406
Studio Bluetooth
Hello,I currently try to download a hcd firmware to ram using Client Control following Doc. No.: 002-16618 https://www.cypress.com/file/462731/download... Show More
StN__1917156
Studio Bluetooth
Is there any hidden disconnect function that accept and a disconnection reason as parameter?all the wiced fuctions wiced_bt_gatt_disconnect , wiced_bt... Show More
BoCo_1857246
Studio Bluetooth
I'm following the instructions in the CyBluetool User guide for activating the transmit tests. Even though the device under test (DUT) returns "succes... Show More
AlGo_4347736
Studio Bluetooth
Hello! Can I use SPI instead of HCI UART to download the application? And if so, where can I read it, how can I do that? Show More
StN__1917156
Studio Bluetooth
Where could see details or example for wiced_bt_l2cap_update_ble_conn_params: in what units are min_int, max_int, timeout and what are min/max values ... Show More
Forum Information

Studio Bluetooth

Discussion forum regarding WICED Studio Bluetooth topics.