Studio Bluetooth Forum Discussions
We had tried to compile and execute the watch demo example program given in the wiced studio ide. It is working with sine wave and giving audio. but when we tried to change the audio source from sine wave to local file (i.e .wav ), we are not able to listen expected sound (some humming sound is coming).
Can you please tell me whether it supports .wav files or .mp3 files and also explain me the process to play those files.
Regards,
Ameet
Show LessHi,
I have a MCU to connect Cybt-343026-01 via puart. I want to upgrade bt modul’s FW. For example, puart receive a defined command, then transmit the needed fw data via puart. Is it Ok? I know I can use HCI uart command, but now I just connect mcu to bt via puart. and I see “wicked-hci-protocol” and “hci-uar-spi-bridge“ exampl, need SPI? I’m confuse.just connect mcu to bt via puart ok or no? or need other hardware pin needed?
Show LessHi,
We have developed a medical device with cyw20719 bluetooth chip. we want to go for FCC compliance certification testing.
In FCC testing we want to change some Bluetooth settings like TX POWER and HOPPING SEQUENCE.
Kindly provide any tool or documents useful for this testing.
Thanks,
Sarathkumar S
Show LessHi,
I want to test one central to connect many peripherals function. So I use device A(Hello_client) to do the testing. Device B(Hello_sensor) is OK for the connection. And I use APP in my mobile to simulate the pheripheral(C). A can search it. But when connect to it. It fails. And I tried with other mobile to simulate central to connect to C, it is OK. I think it maybe the keys is the problem cause. But I don't know how to fix this problem in Hello_client code. Can you help me?
Below is the failure for A to connect to C.
Show Less
Hello,
I tested the A2DP sink function using "snip.bt.a2dp_sink" in WICED-Studio-6.4.
Program to CYBT-343026-01, connect the I2S output to the DAC (NXP UDA1334A), and output to the headset for playback.
The sound output has a noise, once every four seconds, pronounced like "po".
I have tried programming to CYW920706WCDEVAL and the situation is the same.
Is there any experience in solving this? What parameters can be improved?
Show LessHi,
I have a requriement want to have a confirm. There are bluetooth A and B C D. BT A searched B, then create communication with B and transfer data with B. Then can BT A still search other devices such as C, D simultaneously?(which means A communication with B and at the same time , A search tag C and D).
I now have cybt343026-01 module, other module will be OK for above function.
Show LessHi
I am using the CYW920719Q40EVB-01 evaluation kit
I already finish the following items.
1. Create a new project in WICED with just one file which is empty:
#include "sparcommon.h"
APPLICATION_START() {}
2. Download this project from WICED onto your board.
I could sending commands with CyBluetool, and received the correct event.
11/28/19 18:09:19.115 com8 <c Reset
HCI Command Complete Event
com8@115200
[0E 04 ]: 01 03 0C 00
event = 0x0E (14,"Command Complete")
Num_HCI_Command_Packets = 0x1 (1)
Command_Opcode = 0xC03 (3075, "Reset")
Status = 0x0 (0, "Success", "Success")
But if i use other UART console AP, sending the command "01 03 0c 00"
Why i can't receive any feedback by UART console AP?
Have any other setting or initial command to do?
Show LessHi :
today I meet a strange question that my CYW920735Q6EVB-01 board can't print debug message. I have verified the Uart hardware is good, and the Baud rate is correct.
I use the SDK version is 6.4.61
I use the WICED_BT_TRACE("XXXXXXXXXXXXXX", ) to print the debug message , but it can't print the message
but I can use the HCI UART to download firmware
thanks!
mandy
Show LessDuring the loading of an application to the CYBT-343026 module (20706 based), are there any parameters that can be given to Chipload.exe to set the BDADDR of the module? The application is based on the headset demo app.
Show Less