Studio Bluetooth

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
hushilun
Studio Bluetooth

20706使用SDK下的audio->headset,复位后不会自动连接,我想在复位前断开连接,不知道改什么代码?

LiLe_3234306
Studio Bluetooth
Hi, I have a question about "user_data" parameter in interrupt handler.In the prototype of wiced_hal_gpio_register_pin_for_interrupt() API, 3'rd param... Show More
davethecipo
Studio Bluetooth
Hi, I am running the A2DP sink example on CYBT-343026-EVAL board. I play a 48kHz (sample rate) test audio file from a Pixel 4A android device. The osc... Show More
Nagarjuna_k
Studio Bluetooth
Hello All,      I was trying to implement a new use case in which audio data has to be processed by codec DSP. so with SPI  I am trying to read audio ... Show More
hyhw_4628441
Studio Bluetooth
i used the API of "wiced_hal_write_nvram" for write to nvram about 132byte. but, sometimes it is fail with 0x004 error code. my code is as below.   by... Show More
gokulnath
Studio Bluetooth
Hello!I'm new to bT domain and I'm based in France & would like some assistance to choose the perfect Cypress module for my application.   My use case... Show More
GrCa_1363456
Studio Bluetooth
Is there a way to determine if a specific chip or module can support multiple simultaneous BLE Central and Peripheral connections?Sheetal did a nice j... Show More
aglier
Studio Bluetooth
Hi,   I'm using the CYBT 423028-02 on your evaluation board with EZSerial 1.0.4.21 installed. When I try to connect to a device that prefers 2M Physic... Show More
LarryLi-cn
Studio Bluetooth
Hi ALL:  I'm trying to compiling the '20706-A2_Bluetooth' exampel project for CYBT-343026-EVAL following the guide document(AN223400)using with WICED-... Show More
jbiemar46456
Studio Bluetooth
Hello, I'm porting WICED to a STM32H733 and I've an issue with the code snip.bluetooth.ble_gatt_db.c. The function "wiced_bt_stack_init( ..);" is not ... Show More