Studio Bluetooth Forum Discussions
Hi,
通过文档知道cybt342026-01的flash分配如下
1. 我明白DS1和DS2是存放应用程序(.bin)的地方。那么ss的地方是存放哪个DS是active的,对吗?ss的地方还会存储哪些信息?
2. VS1和VS2是存放什么内容的?
3 带OTA_FW_UPGRADE=1和不带这个宏所编译出来的.hex的结构不同,改怎么理解?截图如下
带宏:为什么会分为两个部分?
不带宏:
4 蓝框里的信息应该是存储在了ss的地方,对吗?里面包含的每个byte的意思可以具体说一下吗(比如我看里面是有mac地址的)
带宏:
不带宏:
Hi cypress,
Since CYW20719 supports DLE ( data length extension ), how could I send a large number of data? Is there an API in CYW20719 SDK for this purpose?
Thanks
Show LessHi all:
now I am not very clear about that how the LPN device is to be added into the Bluetooth mesh networking. as we know, the LPN device must need a friend node
to communication with other devices. now the LPN how to choose the networking friend node device. if the provisioning procedure of the LPN device requires the participation of the friend node.
now I download the mesh provision client firmware into the CYW20735Q60EVB-01 board and use the mesh client control to create a Bluetooth mesh networking.
I add a dimmable light device into the networking. the dimmable light can be controlled by mesh client control. finally I configure the mesh light ctl server to LPN node
the configuration as below:
.features = WICED_BT_MESH_CORE_FEATURE_BIT_LOW_POWER, // A bit field indicating the device features. In Low Power mode no Relay, no Proxy and no Friend
.friend_cfg = // Empty Configuration of the Friend Feature
{
.receive_window = 0, // Receive Window value in milliseconds supported by the Friend node.
.cache_buf_len = 0, // Length of the buffer for the cache
.max_lpn_num = 0 // Max number of Low Power Nodes with established friendship. Must be > 0 if Friend feature is supported.
},
.low_power = // Configuration of the Low Power Feature
{
.rssi_factor = 2, // contribution of the RSSI measured by the Friend node used in Friend Offer Delay calculations.
.receive_window_factor = 2, // contribution of the supported Receive Window used in Friend Offer Delay calculations.
.min_cache_size_log = 7, // minimum number of messages that the Friend node can store in its Friend Cache.
.receive_delay = 100, // Receive delay in 1 ms units to be requested by the Low Power node.
.poll_timeout = 10, // Poll timeout in 100ms units to be requested by the Low Power node.
.startup_unprovisioned_adv_to = 128 // Interval in seconds of the advertisments of unprovisioned beacon and service on startup. Value 0 means default 30 seconds.
},
when I want to add the device into the networking. the mesh client control output print messages is below:
it seems the provisioning procedure is failure, now I don't know how to solve this problem !
thanks!
Mandy
Show LessHi all,
i am using CYBT-343026-01 module interfacing with msp430. i want to ask how to communicate both the device with RX and T pins or i need RTS and CTS pins aslo. and how to use hci commands?
thank you.
Show LessWe have a development project to design a Pulse Oximeter capable of BLE and BR performance. Cypress module CYBT-423028-02 looks to be a good fit.
Question 1: Is the stack running on the CYBT-423028-02 or do I need to run the stack on a separate microcontroller?
Question 2: Our application requires a number of security features including secure boot which ensures that only authenticated software can run on the module. Does the CYBT-423028-02 support this?
Show LessHello,
I haven't been able to connect the node for a while from MeshClient.
Here is fragment of log:
17:58:37.744 Net transmit set addr:0001 count:3 interval:50
17:58:37.760 Net Transmit Status from:1 count:3 interval:50
17:58:37.775 Default TTL set addr:0001 TTL:63
17:58:37.775 Default TTL Status from:1 TTL:63 Received TTL:63
17:58:37.807 Beacon set addr:0001 state:0
17:58:37.807 Beacon Status from:1 state:0
17:58:37.807 Network opened
17:58:37.822 done
17:58:43.197 Proxy Connect type:1
17:58:50.209 Net Connect Proxy Connection status provisioner:0 connected:0 over_gatt:1
Does exist a workaround.
Thanks.
Show LessHello,
In the mesh_sensor_publish_timer_callback there is following instruction:
meshmesh_sensor_current_value = mesh_sensor_get_current_value();
Here is definition of mesh_sensor_get_current_value function:
int32_t mesh_sensor_get_current_value(void)
{
return presence_detected;
}
But I didn't find where presence_detected is assigned ???
Any comments ?
Thanks
Show LessHello,
Actually the only option allowing MeshClient application (running on Windows) to receive messages from Sensor Motion node is to specify "all-nodes" value for "Send sensor measurement" parameter. But if I want Sensor Motion to send data only to MeshClient, how to proceed ?
Thanks
Show LessHello,
I've observed that after about 3 min. the connection with Sensor Motion node breaks and Link Staus:0 appears in Log window.
Any comments ?
Thanks.
Show LessHi,
We would like to using evb J18 Uart to connect a main ic evb like microchip evb,
is there a way have simple this uart connection test using using wiced studio?
thanks
Show Less