Studio Bluetooth Forum Discussions
Hello,
What is "Level" property in Mesh Client application (running on Windows) ?
With specified parameters for Lightness, Hue, Saturation I got a certain color on the CYBT-213043-02 module, running Color Light application.
With Lightness=48000, Hue=40000, Saturation=60000, the color on the board is rather turquoise.
But when I introduce these parameters in HSL-to-RGB convertor, found on Internet, the color is yellow.
So, the parameter Level has some influence on the color ?
Thanks.
P.S. The design of interface in Mesh Client is quite strange: Lightness property appears two times: single and together with Hue and Saturation.
Show LessHello,
For example, I didn't find the description of type wiced_platform_button_config_t.
Probably there are a lot of types/functions that aren't documented.
Thanks.
Pavel.
Show LessHello,
The read_me.txt file in Mesh Low Power Led Application contains following phrase:
For low_power_led lpn system node, add LOW_POWER_NODE=1 in Make Target
Should I add this in .c code (using define) or in makefile (which syntax).
Thanks.
Show LessHi
The customer confirmed the UART Timing on the datasheet of [CYBT-343026-01] and
focuses the Max value of the UARTsetupTiming is 10ns.
They think the value is not the max, should be the minimum.
Could you help me confirm the value is the max or minimum?
Thanks
Yang
Show LessHello
How do I specify my own user passkey?
Is there a sample of how to use it?
The development environment is as follows.
CYW43438 & WICED-Studio-6.4
When we will connect CYW920719 board to linux machine we will get 4 interfaces like
ttyUSB1
ttyUSB2
ttyWICED_HCI_UART1
ttyWICED_PUART2
What is the use of 4 interfaces? Why they provided 4 interfaces?.
Show LessMy aim is to send the Hci commands to the CYW920719 board with the help of the python script. CYW920719 board must act as Bt controller and with help of python module pyusb whether i can able to send the HCI base band commands and get the events?. To achive this how i should configure CYW920719 as a BT controller?.
Show LessIs there any appliction in wiced studio to bring up the CYW920719 board in Hci mode. Means we can build that image into the board and get the board in HCI mode. Where we can send the HCI commands through python script.
Show LessHello guys,
I would like to use PUART connected trought external FTDI adapter to my PC insteand of USB port and power the board externellay with 3.3V.
I need to do this operation to verifiy some things before to connect the board to my MCU.
I tried many combination, but without success.
Is possible to do this?
Can you help me?
Thanks.
Best regards.
Show Less