Studio Bluetooth Forum Discussions
Hi,
I found this post in the forum about issues with scan response packages:
I'm also using the CYBT-343026-01 but with newer firmware: 1.2.29
Complete response from module on /qfv: @R,002C,/QFV,0000,E=01021D1D,S=05020016,P=0103,H=D1
Now when my peripheral advertises exactly 7 bytes (flags + incomplete service list) and my scan response does not exceed 24 bytes (<=31 bytes in total) I will see a scan response event with Type = 4 and the complete local name data.
But if the advertising has more then 7 bytes (flags + incomplete service list + tx power level) and the scan response stays at 24 bytes (complete local name) I will receive a scan response event with type 4 but it does not contain the complete local name.
I will add a wireshark log to show you, that the advertisement and scan response of the peripheral is correct.
Has the issue in the above linked thread been fixed in version 1.2.29?
When will the fix be available?
Best regards
Alex
Show LessIs the Firmware download for page 9 1.6 in "CyBluetool User-Guide.pdf" also required for the 343026 evaluation board?
If necessary, please give me the FW.
Is it okay to recognize that + 12dBm cannot be set with mbt.exe for the Radio TX Test item?
Hi everyone
About WICED / MBT.exe
Communication often fails during HCI UART communication.
Can you analyze the cause to help us? Also, can you take measures against it?
(The success rate is high after recovering with the button and after mbt reset.)
Thanks
Yang
Show LessHi,
At the time of shipment, what BD address is already written in CYBT343026?
Is it possible to write a custom BD address before the shipment?
Thanks,
Show LessHi,
The manufacturing test tool "mbt.exe" is a Windows platform application.
We need to handle the test from non Windows platform. So please tell us the way to the test without mbt tool.
Thanks,
Show LessHello,
I am evaluating the CYBT343026 module and have a question.
I tried to send I2S data using BLE notification, but I2S data is unable to get from application, so I'm trying it without application.
Is it possible to send I2S data directly to BLE payload without going though the application such as HFP profile of Bluetooth classic?
Regards,
Show LessHi, do the wiced sdk support dual handsfree SLC connections? The use case is that a headset can be connected to two phones at the same time.