Studio Bluetooth Forum Discussions
HI CYPRESS:
We can't find gap_start_scan() in CYBT-343026-01 user guide , please advice how we get the advertising bluetooth device name with CYBT-343026-01?
Show LessHello!
Working with the board CYW920719Q40EVB-01.
Is there any interface or any way to determine the type of Bluetooth chip restart that has occurred (manual reset, BT watchdog triggered etc.)?
I could not find this information in examples and documents.
Show LessHi,
How to download code to CYW20719 On Chip Flash with WICED?
Thanks
Hi,
Our customers will get BT SIG certification on CYW43438 + WICED.
We planed to use 115853 with reference to the following:
>> https://community.cypress.com/message/186649
However, according to the Japanese certification body, this TCRL2017-2 is old and has specified that the latest TCRL2019-2 needs to be evaluated.
I think Cypress needs an update to 2019-2, are there any plans for an update?
Regards,
Show LessHi,
I am trying to develop an application which supports AVRCP target functionality.
I use CYBT-343026-01 module and develop in Wiced studio 6.4.
my question is:
Do Wiced studio libraries support "AVRC Target Begin Fast Forward" and "AVRC Target End Fast Forward" events described in the WICED HCI UART Control Protocol document?
I want to know that when an AVRCP controller sends "fast forward" command, how Wiced studio libraries handle it.
I briefly looked into the source code below, I could not find the place that handle such command...
20706-A2_Bluetooth/libraries/common/avrc_target/wiced_bt_avrc_tg.c
Regards,
Kazushi
Show LessHi.
I am developing customized HandsFree with CYW20706.
Develop based on WICED's demo / handsfree source.
However, this demo source has a problem with the auto re-connection with iPhone.
When downloading the F/W to Cypress and connecting HandsFree to the iPhone for the first time,
it takes about 4 seconds for iPhone to recognize 'Not connected' when Cypress is powered off.
After Cypress is powered on and automatically connected to iPhone,
it takes about 20 seconds for iPhone to recognize 'Not connected' when Cypress is powered off.
If the iPhone doesn't recognize 'not connected' for 20 seconds,
it won't connect even if you try to connect it after powering on Cypress.
After 20 seconds, even if iPhone recognizes it as 'not connected', it will not auto re-connect.
I tested iPhone 7 and X.
Please let me know if there's a good way to quickly disconnect and reconnect to iPhone.
Show LessHi,
Is CYW920719 board supports USB interface.?
Hi
A customer is considering adopting the CYBT-333032-02 module.
Could you give me some information for profiles of this module?
Could you recommend WICED or Modus 2.0 for your development environment?
I haven't found the weight of this module, could you please tell me the weight?
Thanks
Yang
Show LessI am using the CYW920706WCDEVAL board, and I want to see the buffer data that goes into the data in pin on the board. I loaded the hci.hands_free bluetooth demo code and attached a SPH0645 I2S microphone to it, but we are not getting the microphone to work so we thought it would help to see the data being transmitted.
How would I go about modifying the code in the snip.bt.hci_handsfree demo to view the buffer data?
Show LessHi,
我们想测一下蓝牙的性能,然后找到有一份Manufacturing Bluetooth Test Tool.pdf的文档,但是这份文档的测试都是针对BR/EDR的,那么LE呢?LE该怎么测试? LE有Connectionless DUT Loopback Mode吗?请尽快给与支持。谢谢
Show Less