Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth

Recent discussions

Sort by:
jpaik
Studio Bluetooth
I have faced MIC(Message Integrity Check) error for LE connection. I can see same issue on following link, could you help how to resolve? For more inf... Show More
hyhw_4628441
Studio Bluetooth
Hello, I have questions about operation of HID Device. I tried to test with two of laptops, it is different to operate on HID connection each laptops.... Show More
sylvain_77176
Studio Bluetooth
Hello infineon community, I am contacting you because we are not able to program the CYBT343026-01 that is used on our prototype, The configuration is... Show More
ilHw_4713311
Studio Bluetooth
@Hello.I review CYW20706 and  found that I cannot use i2c and PUART flow control. because puart flow control shares i2c.Or can you tell me how I can c... Show More
PeDo_4684411
Studio Bluetooth
I am using a RS232 FTDI adapter to download a hello_sensor_app through the HCI interface. The communication goes fine and the minidriver is launched O... Show More
user_4767881
Studio Bluetooth
I want to wire a CYBT-353027-EVAL to the CODEC MAX 98090 via I2S running the Headset Demo Application.Try #1: CYBT-353027 is I2S MasterI programmed th... Show More
YaTr_3516311
Studio Bluetooth
Hi,我想把hci_audio_gateway demo里的hci_ag_cfg_settings里的ble_scan_cfg.high_duty_scan_duration=0设置成永远都在high scan,但是测试下来以后,好像scan了一轮后就不scan了。如下是我的的配置。请帮我确认一下 Show More
kf
Studio Bluetooth
In our existing project we use CYBT-353027-02 module and WICED Studio 6.4. The CYBT module is running in embedded mode. The module is connected to a h... Show More
MaRi_1281436
Studio Bluetooth
Hi there. I'd like to know if the CYW20706 can be used directly via HCI H4 (ignoring the WICED Bluetooth stack on the chip) with a full stack on the m... Show More
김삼현
Studio Bluetooth
Cypress_FOTA_release-v3.1.0 or btsdk-peer-apps-ota-master OtaUpgrade 프로젝트 진행 Cypress PuriCare Mask기기 제품 등록중 file load성공후 Upgrade 버튼 클릭시 "Invalid WICED... Show More