Studio Bluetooth Forum Discussions
Hi everyone
I would like to authenticate with SIG. Please let me confirm the information when making an application.
Is the QD ID to be registered 99198 correct?
Thanks
Show LessHello
We are referring to the following document to conduct RF testing.
====
- Infineon-AN214799_Bluetooth_Manufacturing_Test_Tool_for_WICED_Devices-ApplicationNotes-v07_00-EN.pdf
- Chapter 11/page 16
This test issues the commands necessary to configure the Cypress SoC BT device into a test mode for BQB RF testing using a Bluetooth tester, see BQB RF Test Setup [3].
====
Where can we refer to the BQB RF Test Setup [3]? Please release the document.
Thanks,
Show LessHi,
I tried to test the LE OTA Apps for Android, which is in .\WICED-Studio-6.4\common\peer_apps\ota_firmware_upgrade\Android\LeOTAApp\app\build\outputs\apk\app-debug.apk.
By the way, when I "Connect" button to search target LE device, the Apps is down(killed). The issue was always reproduced on my side. For your information, I tested it with Android 9 and 11 version and the test results was same.
I am not sure if the issue is known issue. If so, could you release patched Apps for Android?
One more thing, I also tested with LE OTA Apps within Modus SDK, but it's also killed.
Thanks,
Liam
Show Less
Hi,
I'm using the HCI Uart to send and receive commands from my host computer to the CYBT module.
I also managed to see Trace output generated by "WICED_BT_TRACE" via BTSpy on PUART.
However, when I enable HCI Trace I will receive alot of HCI Trace Events on my HCI Uart. But I can't interprete these data.
I would like to let BTSpy interprete those events. How can I forward those HCI Trace Events to the PUART? Will BTSpy be capable of interpreting the data?
Best regards
Alex
Show LessDear Cypress
I want to know if there is a way to play the tone through I2S.
As an example, when a user presses a button, I want to output pre-defined wav data to I2S.
Please refer to below for detailed conditions:
- H/W : CYW920706WCDEVAL
- S/W : It doesn't matter if it is WICED or MODUS
Thanks in advance.
Show LessI am using a CYW20706 based module (CYBT-343026). I am using the modus toolbox example Audio_Sink for the CYW920706WCDEVAL platform. The only changes I've made are to the wiced_platform.h to update the pinout for my PCB.
The problem is I get a periodic click when streaming from ios. I do not see the issue with android. The period of the click changes on each bluetooth connection, but stays the same while connected. Somewhere between 1 and 2 sec. Some connections do not click at all.
I highlighted in white the click while playing a 20Hz tone using a freq generator app. The second pic is a zoomed in shot.
I then captured the i2s data using a logic analyzer and decoded it to see if it was in my audio circuit or in the data. After decoding I do see the same shapes in the i2s output from the module.
I have verified both android and ios are negotiating the same 44.1kHz, max bitrate=53, joint stereo connections. I'm not sure what to do from here.
What settings can I make to fix this?
Thanks,
Mark
Show Less
Hello,
I'm porting WICED to a STM32H733 and I've an issue with the code snip.bluetooth.ble_gatt_db.c. The function "wiced_bt_stack_init( ..);" is not working.
I've this:
00:00:00.023000 GKI_create_task func=0x80932f9 id=1 name=BTU stack=0x0 stackSize=4096
00:00:00.031000 GKI_create_task func=0x8094ae5 id=0 name=HCISU stack=0x0 stackSize=3072
00:00:00.040000 --
00:00:00.042000 SENT Command to HCI. Name: HCI_Reset (Hex Code: 0x0c03 Param Len: 0) Ctrl(0)
00:00:00.051000 --
00:00:04.042000 --
00:00:04.044000 SENT Command to HCI. Name: HCI_Reset (Hex Code: 0x0c03 Param Len: 0) Ctrl(0)
00:00:04.052000 --
I change platform files but nothing happens on BT_REG_ON or UART_TX.
Do you know were I can found the code to recompile and perform step by step debugger?
Thank you,
Jean
Show LessI have an A2DP device (cyw20706) that does not always reconnect to ios when disconnected. Is there a way to attempt a reconnect from the device?
Show Less