Studio Bluetooth Forum Discussions
Hi all,
Customer needs to have Default Firmware ECCN# of CYBT-333032-02 .
We know that Hardware of CYBT-333032-02 ECCN# is 5A992.C.
We would like to know Default Firmware ECCN#.
BR,Uehara
dear sir/madam,
i was installed wiced studio in new pc(windows 8.1) after installing studio i given build(by double clicking the make file demo.hello_sensor-CYW920706WCDEVAL download)
but in build i got below message
Converting CGS to HEX...
**** Conversion failed ****
Creating OTA images...
**** Conversion failed ****
plz give me slolution for this
thanks.
Show Lessdear sir/madam,
i was installed wiced studio in new pc(windows 8.1) after installing studio i given build(by double clicking the make file demo.hello_sensor-CYW920706WCDEVAL download)
but in build i got below message
make file: demo.hello_sensor-CYW920706WCDEVAL download
Converting CGS to HEX...
**** Conversion failed ****
Creating OTA images...
**** Conversion failed ****
make file: demo.hello_sensor-CYW920706WCDEVAL download VERBOSE=1
make.exe[1]: Leaving directory 'C:/Users/Quantum/Documents/WICED-Studio-6.2/20706-A2_Bluetooth/Wiced-BT/spar'
if not exist build\eclipse_debug\ mkdir build\eclipse_debug\
"../wiced_tools/common/Win32/cp.exe" -f build/hello_sensor-CYW920706WCDEVAL-rom-ram-Wiced-release/A_20703A2-hello_sensor-rom-ram-spar.elf build/eclipse_debug/last_built.elf
"../wiced_tools/common/Win32/echo.exe"
echo Converting CGS to HEX...
Converting CGS to HEX...
..\wiced_tools\CGS\Win32\cgs.exe -D platforms/ -A 0xFF000000 -B platforms/CYW920706WCDEVAL/CYW920706WCDEVAL_SFLASH.btp -I build/hello_sensor-CYW920706WCDEVAL-rom-ram-Wiced-release/hello_sensor-CYW920706WCDEVAL-rom-ram-Wiced-release.hex -H build/hello_sensor-CYW920706WCDEVAL-rom-ram-Wiced-release/hello_sensor-CYW920706WCDEVAL-rom-ram-Wiced-release.hcd --cgs-files build/hello_sensor-CYW920706WCDEVAL-rom-ram-Wiced-release/A_20703A2-hello_sensor-rom-ram-spar.cgs > build/hello_sensor-CYW920706WCDEVAL-rom-ram-Wiced-release/cgs2hex.log 2>&1 && echo Conversion complete || echo **** Conversion failed ****
**** Conversion failed ****
"../wiced_tools/common/Win32/echo.exe"
echo Creating OTA images...
Creating OTA images...
..\wiced_tools\CGS\Win32\cgs.exe -D platforms/ -O DLConfigFixedHeader:0 -B platforms/CYW920706WCDEVAL/CYW920706WCDEVAL_SFLASH.btp -I build/hello_sensor-CYW920706WCDEVAL-rom-ram-Wiced-release/hello_sensor-CYW920706WCDEVAL-rom-ram-Wiced-release.ota.hex --cgs-files build/hello_sensor-CYW920706WCDEVAL-rom-ram-Wiced-release/A_20703A2-hello_sensor-rom-ram-spar.cgs > build/hello_sensor-CYW920706WCDEVAL-rom-ram-Wiced-release/cgs2hex.log 2>&1 && echo Conversion complete || echo **** Conversion failed ****
**** Conversion failed ****
plz give me slolution for this
thanks.
Show LessHi,
Could anyone please suggest how to resolve the status response is unreachable to few server nodes. Let me describe the system configuration to elaborate the problem being faced with CYW20706 devices. I have taken 5 lightness server nodes, a lightness client and a mobile application to provision.
I am sending the following messages from client
1. Status request (every 30 seconds) by passing network address 'C000', i used to get status of all server nodes
2. Every 10 sec, Send set value message first and then immediately status request by passing individual address , i used to get status of corresponding server node
The status messages of all server nodes being received to client for few minutes then one or two server nodes goes unreachable for status request but unfortunately it executes set value message. Yes it works set message to status unreachable nodes if i send 100% brightness or even tried different values between 0-100%. Please note that all devices kept within 1 meter distance.
Please advice to improve system performance as this is for cloud based smart lighting application and need response from all server nodes.
Best regards,
Niresh
Show Lessi need to change device name on runtime and store in flash. actually i use api hci_control_handle_set_local_name
but here device name lost when i am restart the device.
so i need to change and store the name without losing when i am restart the device
Show LessHi Sir,
When I use "demo.hello_sensor-CYW920706WCDEVAL DIRECT_LOAD=1 build" to generate hello_sensor-CYW920706WCDEVAL-rom-ram-Wiced-release.hcd
then use client control to download hcd to ram, hello_sensor can work and I can see the log from uart.
When I use another make :"demo.hello_sensor-CYW920706WCDEVAL download", besides hex file, I also can get "hello_sensor-CYW920706WCDEVAL-rom-ram-Wiced-release.hcd",
then I also use client control to download this hcd to ram, but hello_sensor can not work and I can't see any log from uart.
What is the hcd different between "DIRECT_LOAD=1" and "download"?
Can we use the hcd generated from "download" to download it to RAM?
Show Lessi need to store some 100 bytes of non volatile data in cybt-343026 flash and i need to read and write the data on runtime.
i know the memory layout of cybt-343026 but in which address i need to store and which API i need use i am having doubt can any one help regarding this one.
Show LessHello,
I want to use low power mode in cybt-343026-01. According to datasheet.
1. I have included. Wiced_power_save.h in my application.
Then wiced_sleep_config(WICED_TRUE, NULL, NULL); by doing so I can reduce my current consumption to 3.6mA to 4.6 mA. On power up first it takes 6.9 mA for high duty advertisement. But I want to reduce my current consumption to uA when inactive? I am confuse which mode currently my module is?
2. All unsued Gpio must be in Hi-Z state. So if I am not doing configuration to the unused GPIO, it automatically goes into HI-Z state? Am I correct?
3. When I use wiced_power_save_start(Wiced_WAKE_SOURCE_TIMEOUT,0,0); API it puts the device into HID-OFF state. But in sleep mode I am consuming more current 12 mA. Is it because of my hardware circuitry consuming more current when my module is off or I am doing some mistakes while using low power modes?
Thank you.
Show LessHi,
Now, I can configure the GPIO successful, but I don't know how to put the desired frequency that come from ACLK. Can you give me some advice? Looking forward to your reply! how to put aclk_output_frequency to GPIO.jpg Have a good day to you!
Show Less
hi sir/medam,
when i am sending data from cybt-module to remote bt bluetoothit is allowing only 16 byes. if i am try to send more then 16 bytes it showsing "no mem" message on trace;
can any one having solution for increasing buffer size for data sending from cybt-module to remote bluetooth
Show Less