Studio Bluetooth Forum Discussions
Hello,
I am using WICED Studio 6.2 with CYBT-343026-01. I have around 400 CYBT-343026-01 modules and I want to flash my firmware into it. how can I flash my firmware in all CYBT-343026-01 without connecting to the computer? Is there any external device for OTA? or can I use 1 CYBT-343026-01 as a host device to flash all other modules?
How can I do this please help me.
Thanks in advance
Regards,
Neeraj
Show LessHello,
I was able to write in the following communities.
[EZ-Serial Firmware for CYW2070x-based Modules] In Custom Local GATT, Write properties
This time, let me check how to create multiple Characteristics for one Service.
[SERVICE] /CAC,T=00,P=02,L=0012,D=002800B10C2000089A9EE21115A133333365
[Characteristics of READ] /CAC,T=00,P=02,L=0015,D=032802180001B10C2000089A9EE21115A133333365
[Attribute] /CAC,T=01,P=86,L=0001,D=01
[Characteristics of WRITE] /CAC,T=00,P=02,L=0015,D=032808180002B10C2000089A9EE21115A133333365
[Attribute] /CAC,T=01,P=8A,L=0001,D=00
After the above settings, I checked the /DLD command.
--------
:
:
@E,0024,DL,H=0016,R=001A,T=2800,P=00,U=0028
@E,0024,DL,H=0017,R=0018,T=2803,P=02,U=0328
@E,0040,DL,H=0018,R=0000,T=0000,P=02,U=01B10C2000089A9EE21115A133333365
@E,0024,DL,H=0019,R=0018,T=2803,P=08,U=0328
@E,0040,DL,H=001A,R=0000,T=0000,P=08,U=02B10C2000089A9EE21115A133333365
--------
[Question]
Shouldn't the part written in red be "R = 001A"?
When I executed Write from the Central (iPhone) app, the Handler of Write Event was "001A".
Best regards
上記の設定の後、/DLDコマンドを確認しました。
Show LessHello,
I am using the EZ-Serial Firmware written in CYBT-343026.
If you execute the command (/ BTI) that starts the inquiry process, you should be able to check the information of peripheral devices.
What is the maximum number of this peripheral device list?
[Reference]
User Guide
[3.3.3 Connecting SPP Service of a WICED Module to Another BT Device]
Best regards
Show LessHello guys,
I have a custom board with cyw20719b2, with a build setup using modus toolboox and wiced bt sdk v2.7.1 fdb3982.
We have 32khz crystal connected, I tired to initialize the rtc like this:
rtcConfig.rtcRefClock = RTC_REF_CLOCK_SRC_32KHZ;
rtcConfig.oscillatorFrequencykHz = RTC_REF_CLOCK_SRC_32KHZ;
rtc_init();
But with this I was getting a compilation error: undefined reference for rtcConfg
I'm able to resolve this issue following instructions from answer to this query on the forum:
The answer suggests this:
However to avoid undefined reference error, please include the below line to C:\Users\anpm\ModusToolbox_2.1\wiced_btsdk\dev-kit\baselib\20719B2\internal\20719B2\patches\patch.sym
rtcConfig = 0x201b21;
With this change I'm able to successfully compile and able to set and get accurate rtc time using provided apis (rtc_setRTCTime & rtc_getRTCTime).
But now I need to use this api "rtc_getRTCRawClock" to get raw rtc time, but now again I'm getting this compilation error:
undefined reference for rtc_getRTCRawClock.
I tried to check if this (rtc_getRTCRawClock) symbol is present in the file:
\wiced_btsdk\dev-kit\baselib\20719B2\internal\20719B2\patches\patch.sym
But the symbol is not present in the above file.
Can you please let me know how do I fix this issue without updating the sdk ?
Do I need to add a symbol into this patch.sym for rtc_getRTCRawClock also ? if yes please provide the details.
thanks,
aniket
Show LessHello,
I would like to confirm the following description in the CYBT-483056-02 datasheet.
https://www.cypress.com/file/511686/download
■ Certified up to +20 dBm for FCC and ISED
■ Certified up to +10 dBm for MIC and CE standards
Checking the Test report, the maximum output power of CE and MIC (Japan) is as follows.
RF Regulatory Certifications for CYBT-483039-02 EZ-BT™ XR Module - KBA224516
[CE]
-BT: 20dBm (Limit)
* 1972087R-RF-CE-EN300328-BT3.0-EZ-BT WICED XR Module with Mesh-CYBT-483039-02, CYBT-483056-02, CYBT-483062-02-V1.0.pdf
-BLE: 20dBm (Limit)
* 1972087R-RF-CE-EN300328-BLE-EZ-BT WICED XR Module with Mesh-CYBT-483039-02, CYBT-483056-02, CYBT-483062-02-V1.0.pdf
[MIC]
-BT: 20dBm [3mW / MHz] (Limit)
* 1972087R-RF-MIC (BT 3.0)-EZ-BT WICED XR Module with Mesh-CYBT-483039-02, CYBT-483056-02, CYBT-483062-02-V1.0.pdf
-BLE: 10dBm (Limit)
* 1972087R-RF-MIC (BT 4.0) -EZ-BT WICED XR Module with Mesh-CYBT-483039-02, CYBT-483056-02, CYBT-483062-02-V1.0.pdf
* 1972087R-RF-MIC (BT 5.0)-EZ-BT WICED XR Module with Mesh-CYBT-483039-02, CYBT-483056-02, CYBT-483062-02-V1.0.pdf
Why does the datasheet limit CE and MIC to 10 dBm?
Can CE and MIC be used with the output Power as per the test report?
Best regards,
Takahashi
Show LessI am trying to create an event to send a Mesh message, but the wiced_bt_mesh_create_event function always seems to return NULL. Does anyone have an idea why this might be or how to fix this?
wiced_bt_mesh_event_t *p_event = wiced_bt_mesh_create_event(
0,
0x0131, // MESH_COMPANY_ID_CYPRESS
0x1000, // WICED_BT_MESH_CORE_MODEL_ID_GENERIC_ONOFF_SRV
0,
0);
I'm reopening this discussion after a long time of giving up on Mesh on this device, here is the older one. I was advised by DheerajP_41 to set the element_idx to 0(from 0x00) and to check if MESH_COMPANY_ID_CYPRESS and the model ID were defined correctly. I have tried those but wiced_bt_mesh_create_event still only returns NULL. I'm attaching my code where I marked my code with comments(// MY CODE BEGIN and // MY CODE END), the rest is just the mesh_onoff_client from snip/mesh/ in the SDK.
The device(CYBT-423028-02) is in a Mesh network containing another CYBT-423028-02 programmed with the mesh_onoff_server example from 20719-B1_Bluetooth/apps/snip/mesh/. I'm provisioning both devices, then I give the Generic OnOff Server and the Generic OnOff Client models the same app key, set both their publish addresses and subscription addresses to the same group(0xC000) but I also tried setting the publish address of the client to 0xFFFF and the unicast address of the server, it didn't change anything and wiced_bt_mesh_create_event() keeps returning NULL.
In case it's relevant, I'm reading the WICED_BT_TRACE outputs using PuTTY and a USB-UART bridge.
I'm just trying to send a set message from the client to the server and change the onoff state right now to keep things as simple as possible. If I should be using another function or go about this a different way, I would be glad if anyone could help me out. I'm also wondering if anyone else can recreate the issue or not.
Show LessHello,
I have flashed the battery server example code from WICED studio 6.4 to CYBT 423028 Eval board, and battery client code to another board.
Not getting response from server.
I want to get the battery status periodically from battery server.
I have created periodic timer (5 Sec ) in Battery Client and in that timer I am calling wiced_bt_mesh_create_event by passing the element index as 0, default Vendor Compony ID and Vendor Model ID, dst as 0, and app_key_idx as 0xffff. Event is getting created I believe, as wiced_bt_mesh_create_event not returning NULL.
Once the event is created I am passing this event to wiced_bt_mesh_battery_client_send_get as an argument, it returns 8019 code.
On server side could not see request is getting received.
Both battery client and server are provisioned through Mehs_Lighting android Mobile application.
Is there any thing I am missing or doing wrong ?
Show LessThis might be a lengthy post an i apologize in advance
I am trying to run a BLE server that transmits around 35-40KBytes/sec through notifications. I have the server and notifications up and running with BlueZ-5.54 interfacing over HCI with BT860 Laird bluetooth module that leverages CYW20704 A2 Chipset.
The problem is with HCI Event: Number of Completed Packets. From what I understand the bluetooth controller will send this event once it has transmitted buffered packets to indicate available capacity. Also it is manufacture specific and cannot be controlled.
The chipset can buffer up to 15 packets of length 251 each. I confirmed that by sending raw command using hcitool.
All good so far, here is the problem description:
1. The applications sends 15 packets to the controller
2. *After 2 x connection_interval_ms* Controller replies with HCI Event: Number of Completed Packets = 2
3. This continues until all packets are sent. At the end, controller sends 8 HCI Event: Number of Completed Packets = 2/1, all 2 x connection_interval_ms apart
I am pasting output from "btmon" here for a better understanding of the situation(the important sections are separated by /*********break-lines******/).
From the output it is clear that the controller only transmits 2 ACL packet at a time and then waits 2xconnection_interval_ms. This really is the bottleneck of my BLE server, please let me know how I can improve it!
I have tried different connection intervals, mtu sizes and even different client apps(nRF connect and RaspberryPi gatt client) all give me the same results. As well as gone through documentation for BT860 and CYW20704.
Can someone please help me understand how I can fix this? Essentially,
1. Why are the packets buffered and not transmitted?
2. If they are being transmitted, why is it not reported by the controller? How do I know if this is a bug in the controller?
3. Why are "Number of Completed Packets" HCI event always 2 x connection intervals apart? How can I control its frequency?
Show Less/********************************************Initiate Connection and GATT Service discovery*****************************************/
> HCI Event: LE Meta Event (0x3e) plen 19 #289 [hci0] 1767.983447
LE Connection Complete (0x01)
Status: Success (0x00)
Handle: 64
Role: Slave (0x01)
Peer address type: Random (0x01)
Peer address: F5:2F:BD:4D:B4:A1 (Static)
Connection interval: 7.50 msec (0x0006)
Connection latency: 0 (0x0000)
Supervision timeout: 4000 msec (0x0190)
Master clock accuracy: 0x07
@ MGMT Event: Device Connected (0x000b) plen 13 {0x0002} [hci0] 1767.983514
LE Address: F5:2F:BD:4D:B4:A1 (Static)
Flags: 0x00000000
Data length: 0
@ MGMT Event: Device Connected (0x000b) plen 13 {0x0001} [hci0] 1767.983514
LE Address: F5:2F:BD:4D:B4:A1 (Static)
Flags: 0x00000000
Data length: 0
< HCI Command: LE Read Remote Used Features (0x08|0x0016) plen 2 #290 [hci0] 1767.983782
Handle: 64
> HCI Event: Command Status (0x0f) plen 4 #291 [hci0] 1767.985754
LE Read Remote Used Features (0x08|0x0016) ncmd 1
Status: Success (0x00)
> ACL Data RX: Handle 64 flags 0x02 dlen 11 #292 [hci0] 1768.003893
ATT: Read By Group Type Request (0x10) len 6
Handle range: 0x0001-0xffff
Attribute group type: Primary Service (0x2800)
> HCI Event: LE Meta Event (0x3e) plen 12 #293 [hci0] 1768.020620
LE Read Remote Used Features (0x04)
Status: Unsupported Remote Feature / Unsupported LMP Feature (0x1a)
Handle: 64
Features: 0xff 0x00 0x00 0x00 0x00 0x00 0x00 0x00
LE Encryption
Connection Parameter Request Procedure
Extended Reject Indication
Slave-initiated Features Exchange
LE Ping
LE Data Packet Length Extension
LL Privacy
Extended Scanner Filter Policies
< ACL Data TX: Handle 64 flags 0x00 dlen 16 #294 [hci0] 1768.020769
LE L2CAP: Connection Parameter Update Request (0x12) ident 1 len 8
Min interval: 24
Max interval: 40
Slave latency: 0
Timeout multiplier: 400
< ACL Data TX: Handle 64 flags 0x00 dlen 18 #295 [hci0] 1768.034943
ATT: Read By Group Type Response (0x11) len 13
Attribute data length: 6
Attribute group list: 2 entries
Handle range: 0x0001-0x0006
UUID: Generic Access Profile (0x1800)
Handle range: 0x0007-0x000a
UUID: Generic Attribute Profile (0x1801)
> HCI Event: LE Meta Event (0x3e) plen 11 #296 [hci0] 1768.043019
LE Data Length Change (0x07)
Handle: 64
Max TX octets: 251
Max TX time: 2120
Max RX octets: 251
Max RX time: 2120
> ACL Data RX: Handle 64 flags 0x02 dlen 10 #297 [hci0] 1768.050522
LE L2CAP: Connection Parameter Update Response (0x13) ident 1 len 2
Result: Connection Parameters accepted (0x0000)
> HCI Event: Number of Completed Packets (0x13) plen 5 #298 [hci0] 1768.058490
Num handles: 1
Handle: 64
Count: 2
> ACL Data RX: Handle 64 flags 0x02 dlen 11 #299 [hci0] 1768.065527
ATT: Read By Group Type Request (0x10) len 6
Handle range: 0x000b-0xffff
Attribute group type: Primary Service (0x2800)
< ACL Data TX: Handle 64 flags 0x00 dlen 26 #300 [hci0] 1768.065867
ATT: Read By Group Type Response (0x11) len 21
Attribute data length: 20
Attribute group list: 1 entry
Handle range: 0x000b-0x0012
UUID: Vendor specific (a79ef145-bde1-4bbd-8fbd-28d5dad70a97)
> ACL Data RX: Handle 64 flags 0x02 dlen 11 #301 [hci0] 1768.081234
ATT: Read By Group Type Request (0x10) len 6
Handle range: 0x0013-0xffff
Attribute group type: Primary Service (0x2800)
< ACL Data TX: Handle 64 flags 0x00 dlen 9 #302 [hci0] 1768.081687
ATT: Error Response (0x01) len 4
Read By Group Type Request (0x10)
Handle: 0x0013
Error: Attribute Not Found (0x0a)
> ACL Data RX: Handle 64 flags 0x02 dlen 7 #303 [hci0] 1768.095555
ATT: Read Request (0x0a) len 2
Handle: 0x000b
< ACL Data TX: Handle 64 flags 0x00 dlen 21 #304 [hci0] 1768.095684
ATT: Read Response (0x0b) len 16
Value: 970ad7dad528bd8fbd4be1bd45f19ea7
> HCI Event: Number of Completed Packets (0x13) plen 5 #305 [hci0] 1768.096516
Num handles: 1
Handle: 64
Count: 2
> HCI Event: LE Meta Event (0x3e) plen 10 #306 [hci0] 1768.103986
LE Connection Update Complete (0x03)
Status: Success (0x00)
Handle: 64
Connection interval: 30.00 msec (0x0018)
Connection latency: 0 (0x0000)
Supervision timeout: 4000 msec (0x0190)
> ACL Data RX: Handle 64 flags 0x02 dlen 11 #307 [hci0] 1768.163413
ATT: Read By Type Request (0x08) len 6
Handle range: 0x0001-0x0006
Attribute type: Characteristic (0x2803)
< ACL Data TX: Handle 64 flags 0x00 dlen 20 #308 [hci0] 1768.163731
ATT: Read By Type Response (0x09) len 15
Attribute data length: 7
Attribute data list: 2 entries
Handle: 0x0002
Value: 820300002a
Handle: 0x0005
Value: 020600012a
> ACL Data RX: Handle 64 flags 0x02 dlen 7 #309 [hci0] 1768.223048
ATT: Read Request (0x0a) len 2
Handle: 0x0003
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #310 [hci0] 1768.223324
ATT: Read Response (0x0b) len 22
Value: 427261696e436f205261737062657272795069205374
> HCI Event: Number of Completed Packets (0x13) plen 5 #311 [hci0] 1768.223995
Num handles: 1
Handle: 64
Count: 2
> ACL Data RX: Handle 64 flags 0x02 dlen 7 #312 [hci0] 1768.313032
ATT: Read Request (0x0a) len 2
Handle: 0x0006
< ACL Data TX: Handle 64 flags 0x00 dlen 7 #313 [hci0] 1768.313294
ATT: Read Response (0x0b) len 2
Value: 8000
> ACL Data RX: Handle 64 flags 0x02 dlen 9 #314 [hci0] 1768.373681
ATT: Find Information Request (0x04) len 4
Handle range: 0x0004-0x0006
< ACL Data TX: Handle 64 flags 0x00 dlen 18 #315 [hci0] 1768.373818
ATT: Find Information Response (0x05) len 13
Format: UUID-16 (0x01)
Handle: 0x0004
UUID: Characteristic Extended Properties (0x2900)
Handle: 0x0005
UUID: Characteristic (0x2803)
Handle: 0x0006
UUID: Appearance (0x2a01)
> HCI Event: Number of Completed Packets (0x13) plen 5 #316 [hci0] 1768.373932
Num handles: 1
Handle: 64
Count: 2
> ACL Data RX: Handle 64 flags 0x02 dlen 7 #317 [hci0] 1768.433025
ATT: Read Request (0x0a) len 2
Handle: 0x0004
< ACL Data TX: Handle 64 flags 0x00 dlen 7 #318 [hci0] 1768.433350
ATT: Read Response (0x0b) len 2
Value: 0100
> ACL Data RX: Handle 64 flags 0x02 dlen 9 #319 [hci0] 1768.493683
ATT: Find Information Request (0x04) len 4
Handle range: 0x0007-0x0006
< ACL Data TX: Handle 64 flags 0x00 dlen 9 #320 [hci0] 1768.493961
ATT: Error Response (0x01) len 4
Find Information Request (0x04)
Handle: 0x0007
Error: Invalid Handle (0x01)
> HCI Event: Number of Completed Packets (0x13) plen 5 #321 [hci0] 1768.493965
Num handles: 1
Handle: 64
Count: 2
> ACL Data RX: Handle 64 flags 0x02 dlen 7 #322 [hci0] 1768.553023
ATT: Read Request (0x0a) len 2
Handle: 0x0003
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #323 [hci0] 1768.553275
ATT: Read Response (0x0b) len 22
Value: 427261696e436f205261737062657272795069205374
> ACL Data RX: Handle 64 flags 0x02 dlen 9 #324 [hci0] 1768.613688
ATT: Read Blob Request (0x0c) len 4
Handle: 0x0003
Offset: 0x0016
< ACL Data TX: Handle 64 flags 0x00 dlen 21 #325 [hci0] 1768.614021
ATT: Read Blob Response (0x0d) len 16
61 72 6b 20 47 41 54 54 20 53 65 72 76 65 72 00 ark GATT Server.
> HCI Event: Number of Completed Packets (0x13) plen 5 #326 [hci0] 1768.614029
Num handles: 1
Handle: 64
Count: 2
> HCI Event: Number of Completed Packets (0x13) plen 5 #327 [hci0] 1768.904932
Num handles: 1
Handle: 64
Count: 1
> HCI Event: LE Meta Event (0x3e) plen 10 #328 [hci0] 1776.593921
LE Connection Update Complete (0x03)
Status: Success (0x00)
Handle: 64
Connection interval: 7.50 msec (0x0006)
Connection latency: 0 (0x0000)
Supervision timeout: 4000 msec (0x0190)
> ACL Data RX: Handle 64 flags 0x02 dlen 11 #329 [hci0] 1788.592219
ATT: Read By Type Request (0x08) len 6
Handle range: 0x000b-0x0012
Attribute type: Characteristic (0x2803)
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #330 [hci0] 1788.592438
ATT: Read By Type Response (0x09) len 22
Attribute data length: 21
Attribute data list: 1 entry
Handle: 0x000c
Value: 100d00072c6b8a1e1aeda86b47cec24ebcd4e8
> ACL Data RX: Handle 64 flags 0x02 dlen 11 #331 [hci0] 1788.607574
ATT: Read By Type Request (0x08) len 6
Handle range: 0x000d-0x0012
Attribute type: Characteristic (0x2803)
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #332 [hci0] 1788.607721
ATT: Read By Type Response (0x09) len 22
Attribute data length: 21
Attribute data list: 1 entry
Handle: 0x0010
Value: 0c110008c6a6034ef06baf8549343533924732
> ACL Data RX: Handle 64 flags 0x02 dlen 11 #333 [hci0] 1788.622590
ATT: Read By Type Request (0x08) len 6
Handle range: 0x0011-0x0012
Attribute type: Characteristic (0x2803)
< ACL Data TX: Handle 64 flags 0x00 dlen 9 #334 [hci0] 1788.622708
ATT: Error Response (0x01) len 4
Read By Type Request (0x08)
Handle: 0x0011
Error: Attribute Not Found (0x0a)
> HCI Event: Number of Completed Packets (0x13) plen 5 #335 [hci0] 1788.623156
Num handles: 1
Handle: 64
Count: 2
> ACL Data RX: Handle 64 flags 0x02 dlen 7 #336 [hci0] 1788.637230
ATT: Read Request (0x0a) len 2
Handle: 0x000c
< ACL Data TX: Handle 64 flags 0x00 dlen 24 #337 [hci0] 1788.637352
ATT: Read Response (0x0b) len 19
Value: 100d00072c6b8a1e1aeda86b47cec24ebcd4e8
> ACL Data RX: Handle 64 flags 0x02 dlen 7 #338 [hci0] 1788.652248
ATT: Read Request (0x0a) len 2
Handle: 0x0010
< ACL Data TX: Handle 64 flags 0x00 dlen 24 #339 [hci0] 1788.652361
ATT: Read Response (0x0b) len 19
Value: 0c110008c6a6034ef06baf8549343533924732
> HCI Event: Number of Completed Packets (0x13) plen 5 #340 [hci0] 1788.653195
Num handles: 1
Handle: 64
Count: 2
> ACL Data RX: Handle 64 flags 0x02 dlen 9 #341 [hci0] 1788.697157
ATT: Find Information Request (0x04) len 4
Handle range: 0x000e-0x0012
< ACL Data TX: Handle 64 flags 0x00 dlen 18 #342 [hci0] 1788.697287
ATT: Find Information Response (0x05) len 13
Format: UUID-16 (0x01)
Handle: 0x000e
UUID: Characteristic User Description (0x2901)
Handle: 0x000f
UUID: Client Characteristic Configuration (0x2902)
Handle: 0x0010
UUID: Characteristic (0x2803)
> ACL Data RX: Handle 64 flags 0x02 dlen 7 #343 [hci0] 1788.712242
ATT: Read Request (0x0a) len 2
Handle: 0x000e
< ACL Data TX: Handle 64 flags 0x00 dlen 18 #344 [hci0] 1788.712447
ATT: Read Response (0x0b) len 13
Value: 4545472052656164696e677300
> HCI Event: Number of Completed Packets (0x13) plen 5 #345 [hci0] 1788.712787
Num handles: 1
Handle: 64
Count: 2
> ACL Data RX: Handle 64 flags 0x02 dlen 7 #346 [hci0] 1788.727224
ATT: Read Request (0x0a) len 2
Handle: 0x000f
< ACL Data TX: Handle 64 flags 0x00 dlen 5 #347 [hci0] 1788.727405
ATT: Read Response (0x0b) len 0
Value:
> HCI Event: Number of Completed Packets (0x13) plen 5 #348 [hci0] 1788.749650
Num handles: 1
Handle: 64
Count: 2
> ACL Data RX: Handle 64 flags 0x02 dlen 9 #349 [hci0] 1788.764653
ATT: Find Information Request (0x04) len 4
Handle range: 0x0012-0x0012
< ACL Data TX: Handle 64 flags 0x00 dlen 10 #350 [hci0] 1788.764773
ATT: Find Information Response (0x05) len 5
Format: UUID-16 (0x01)
Handle: 0x0012
UUID: Characteristic User Description (0x2901)
> ACL Data RX: Handle 64 flags 0x02 dlen 7 #351 [hci0] 1788.779703
ATT: Read Request (0x0a) len 2
Handle: 0x0012
< ACL Data TX: Handle 64 flags 0x00 dlen 18 #352 [hci0] 1788.779898
ATT: Read Response (0x0b) len 13
Value: 4545472052656164696e677300
> HCI Event: Number of Completed Packets (0x13) plen 5 #353 [hci0] 1788.794650
Num handles: 1
Handle: 64
Count: 2
> ACL Data RX: Handle 64 flags 0x02 dlen 9 #354 [hci0] 1790.062100
ATT: Write Request (0x12) len 4
Handle: 0x000f
Data: 0100/************************************************** START THE NOTIFICATIONS **********************************************************/
> ACL Data RX: Handle 64 flags 0x02 dlen 9 #354 [hci0] 1790.062100
ATT: Write Request (0x12) len 4
Handle: 0x000f
Data: 0100
< ACL Data TX: Handle 64 flags 0x00 dlen 5 #355 [hci0] 1790.062426
ATT: Write Response (0x13) len 0
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #356 [hci0] 1790.063602
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 54f003008bce915f8bce915f8bce915f5483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #357 [hci0] 1790.064609
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #358 [hci0] 1790.065696
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #359 [hci0] 1790.066768
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #360 [hci0] 1790.067887
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #361 [hci0] 1790.068955
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #362 [hci0] 1790.070077
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #363 [hci0] 1790.071196
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #364 [hci0] 1790.072277
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #365 [hci0] 1790.073346
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #366 [hci0] 1790.074458
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #367 [hci0] 1790.075560
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #368 [hci0] 1790.076665
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #369 [hci0] 1790.077775
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
> HCI Event: Number of Completed Packets (0x13) plen 5 #370 [hci0] 1790.084497
Num handles: 1
Handle: 64
Count: 2
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #371 [hci0] 1790.084532
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #372 [hci0] 1790.084546
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
> HCI Event: Number of Completed Packets (0x13) plen 5 #373 [hci0] 1790.099497
Num handles: 1
Handle: 64
Count: 2/*******************************************BREAK: SKIP TO END OF TRANSFER ************************************************/
> HCI Event: Number of Completed Packets (0x13) plen 5 #493 [hci0] 1790.736984
Num handles: 1
Handle: 64
Count: 2
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #494 [hci0] 1790.737022
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #495 [hci0] 1790.737037
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
> HCI Event: Number of Completed Packets (0x13) plen 5 #496 [hci0] 1790.751975
Num handles: 1
Handle: 64
Count: 2
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #497 [hci0] 1790.752012
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
< ACL Data TX: Handle 64 flags 0x00 dlen 27 #498 [hci0] 1790.752027
ATT: Handle Value Notification (0x1b) len 22
Handle: 0x000d
Data: 0000000030b6510100000000e8b651015483ac7e
> HCI Event: Number of Completed Packets (0x13) plen 5 #499 [hci0] 1790.766970
Num handles: 1
Handle: 64
Count: 2
> HCI Event: Number of Completed Packets (0x13) plen 5 #500 [hci0] 1790.782000
Num handles: 1
Handle: 64
Count: 2
> HCI Event: Number of Completed Packets (0x13) plen 5 #501 [hci0] 1790.796968
Num handles: 1
Handle: 64
Count: 2
> HCI Event: Number of Completed Packets (0x13) plen 5 #502 [hci0] 1790.811970
Num handles: 1
Handle: 64
Count: 2
> HCI Event: Number of Completed Packets (0x13) plen 5 #503 [hci0] 1790.826973
Num handles: 1
Handle: 64
Count: 2
> HCI Event: Number of Completed Packets (0x13) plen 5 #504 [hci0] 1790.841972
Num handles: 1
Handle: 64
Count: 2
> HCI Event: Number of Completed Packets (0x13) plen 5 #505 [hci0] 1790.856964
Num handles: 1
Handle: 64
Count: 2
> HCI Event: Number of Completed Packets (0x13) plen 5 #506 [hci0] 1791.031954
Num handles: 1
Handle: 64
Count: 1
Hi:
在对CWY20735B1的开发中,发现了在wiced studio环境下对工程编译编译以后,在build目录下生成了xxx.hex与xxx.ota.hex这两个烧录文件, 由于目前不知道这两个烧录文件有什么区别,请问在进行生产的时候,需要烧录哪一个文件!
多谢各位及时回复!
谢谢!
Show LessHello,
I'm trying [3.6.5 Detecting and Processing Written Data from a Remote Client] in the User Guide.
The following settings are made.
[Command]
/CAC,T=00,P=2,L=0012,D=002800B10C2000089A9EE21115A133333365
/CAC,T=00,P=2,L=0015,D=032808180001B10C2000089A9EE21115A133333365
/CAC,T=01,P=8A,L=0001,D=
/CAC,T=00,P=2,L=0012,D=002800B10C2000089A9EE21115A133333365
・T = 00 : Type (0: structure)
・P = 02 : Permission bit (0x02: Readable)
・L = 0012 : Data Length (0x0012: 18Byte)
・D = 002800B10C2000089A9EE21115A133333365 (18Byte)
- 0028 : Attribute type (0x2800: Primary Service Declaration)
- 00B10C2000089A9EE21115A133333365 : Service UUID (0x65333333A11511E29E9A0800200CB100)
/CAC,T=00,P=2,L=0015,D=032808180001B10C2000089A9EE21115A133333365
・T = 00 : Type (0: structure)
・P = 02 : Permission bit (0x02: Readable)
・L = 0015 : Data Length (0x0015: 21Byte)
・D = 032808180001B10C2000089A9EE21115A133333365 (21Byte)
- 0328 : Attribute type (0x2803: Characteristic Declaration)
- 08 : Characteristic properties bit (0x08: Write)
- 1800 : Handle of value attribute (0x0018)
- 01B10C2000089A9EE21115A133333365 : Characteristic UUID (0x65333333A11511E29E9A0800200CB101)
/CAC,T=01,P=8A,L=0001,D=
・T = 01 : Type (1: characteristic value)
・P = 8A : Permission bit (0x02: Readable | 0x08: Write request [acknowledged] | 0x80: UUID is 128 bits??)
・L = 0001 : Data Length (0x0001: 1Byte)
・D =
However, even with this setting, the "W" Event is not issued even if the Write command is issued from the Central App [CySmart etc] after Connection.
[Q1]
What could be the reason why the "W" Event (gatts_data_written ID = 5/2) is not issued?
On the app side, an "Invalid Offset (0x07)" Error will be returned.
Is this a problem?
[Q2]
What is "Invalid Offset (0x07)"?
Is the "/CAC" setting incorrect?
[Q3]
There is no description of "0x80" in the User Guide for the "P" option of "/CAC".
If you check gatts_db_entry_blob (DGATT, ID = 5/4), it says "Bit 7 (0x80) = UUID is 128 bits".
Can I think of "0x80" as a "UUID is 128 bits" permission bit?
Best regards,
Takahashi
Show Less