I have faced MIC(Message Integrity Check) error for LE connection. I can see same issue on following link, could you help how to resolve?
For more information, please refer to the following.
https://community.infineon.com/t5/Studio-Bluetooth/Bug-report-Connection-Terminated-Due-to-MIC-Failure-0x3d-WICED-6/td-p/245462
https://community.infineon.com/t5/Studio-Bluetooth/Bug-report-BLE-cant-reconnect-to-a-bonded-device/m-p/35458#M163
1. Test environment
1) H/W
- Local H/W : CYW920706WCDEVAL
- Peer device :
> LG Stylus2
>> Android version 7.0
>> BR/EDR public BD address : DO:13:FD:50:F8:C8
> HUAWEL P9 lite. (Model number : HUAWEL VNS-L22)
>> Android version 7.0
2) S/W
- SDK : ModusToolBox 2.3 and LE_Hello_sensor application
- SDK LIB : Wiced_btsdk baselib release v3.0.0
- Peer Apps : LightBlue, local developed BLE application.
2. Test procedure
- Step 1. Hello_sensor build & download
- Step 2. Pairing with android phone.
- Step 3. Connection success.
- Step 4. Remote disconnect after pairing success.
- Step 5. Start connection from andoid phone.
- Step 6. Link connection fail due to MIC error. (error code 0x3d)
3. Test Results
- I tested other BLE peripheral with two android phones and it works well. (No MIC error)
- CYW920706WCDEVAL works fine with iphone, and other many android phone.
- HCI fail : HCI_Encryption_Change event status code 0x3d. (mic error)
5. attached log file.
- mic_error_app_log.txt : application log with MIC error.
- mic_error_btspy.txt : MIC error with CYW920706WCDEVAL and LG android phone.
- no_mic_with_iphone.txt : No MIC error with CYW920706WCDEVAL and iphone.
Thanks.
Show LessHello,
I have questions about operation of HID Device.
I tried to test with two of laptops, it is different to operate on HID connection each laptops.
The SW information and test process are as below.
SW Information
- Chipset & EVK : CYW20706 & F1DC2076 EVB (made in F1media)
- WICED SDK version : WCIED 6.2.1
- Test application : HID Device
Test Process
- Connect from Windows PC to F1DC2706(CYW20706)
- Send the HID data.
- Result
#1) it seems that enter to sniff mode normally
Notebook (LG - 15U560)
- manufacturer : Intel Corporation
- F/W version : HCI 8.4096 / LMP 8.4096
- Driver provider : Intel Corporation
- Driver date : 2017-04-07
- Driver version : 19.60.0.3
#2) it seems that enter to sniff mode, but its connect/disconnect to SDP and RFCOMM repeatly,
and also enter/exit sniff mode repeatly by connect/disconnect.
Notebook (LG –15ZD980-GX50K)
- Manufacturer : Intel Corporation
- F/W version : HCI 8.256 / LMP 8.256
- Driver provider : Intel Corporation
- Driver date : 2017-05-04
- Driver version : 20.60.0.4
Snoop Log
- refer to attatched files. its name is written name of laptop.
Why is the different each for laptops? Does it problem of compability?
Or, am i missed anything that need to set?
I want to know why is the different to operate on HID connection.
Please, could you help me anybody who know?
Show Less
Hello infineon community,
I am contacting you because we are not able to program the CYBT343026-01 that is used on our prototype,
The configuration is :
1. Hardware:
we are using the HCI interface of an CYBT-343026-EVAL board, switch are configured to low (if we consider the position given in the screen below) and wires have been soldered to connect eval board to our prototype.
Detail of CYBT343026-01 connection on PROTOTYPE :
uarts, "Reset" and "Recover" pin are connected to a microcontroller that is setting the connected pin to high impedance during flash.
2. Software:
Before starting programming the sequence given below is realized:
“Press and hold the 'Recover' button on the kit.
Press and hold the 'Reset' button on the kit.
Release the 'Reset' button.
After one second, release the 'Recover' button.”
Then ChipLoader programming tool is used to program the CYBT and the result is given below :
C:\Cypress\Wiced_Smart_SDK\WICED-Smart-SDK\Tools\ChipLoad\Win32>ChipLoad.exe -BLUETOOLMODE -PORT COM5 -NOVERIFY -MINIDRIVER C:\Cypress\Wiced_Smart_SDK\WICED-Smart-SDK\Tools\ChipLoad\Win32\minidriver.hex -BTP C:\Cypress\Wiced_Smart_SDK\WICED-Smart-SDK\Tools\ChipLoad\Win32\CYP_TCV4.btp -CONFIG C:\Cypress\Wiced_Smart_SDK\WICED-Smart-SDK\Tools\ChipLoad\Win32\CYP_TCV4_download.hex
Download minidriver successfully had written 249 bytes to address 0x000D0200
Download minidriver successfully had written 249 bytes to address 0x000D02F9
Download minidriver successfully had written 249 bytes to address 0x000D03F2
Download minidriver successfully had written 249 bytes to address 0x000D04EB
Download minidriver successfully had written 249 bytes to address 0x000D05E4
Download minidriver successfully had written 249 bytes to address 0x000D06DD
Download minidriver successfully had written 249 bytes to address 0x000D07D6
Download minidriver successfully had written 249 bytes to address 0x000D08CF
Download minidriver successfully had written 249 bytes to address 0x000D09C8
Download minidriver successfully had written 249 bytes to address 0x000D0AC1
Download minidriver successfully had written 249 bytes to address 0x000D0BBA
Download minidriver successfully had written 249 bytes to address 0x000D0CB3
Download minidriver successfully had written 249 bytes to address 0x000D0DAC
Download minidriver successfully had written 249 bytes to address 0x000D0EA5
Download minidriver successfully had written 249 bytes to address 0x000D0F9E
Download minidriver successfully had written 249 bytes to address 0x000D1097
Download minidriver successfully had written 249 bytes to address 0x000D1190
Download minidriver successfully had written 249 bytes to address 0x000D1289
Download minidriver successfully had written 249 bytes to address 0x000D1382
Download minidriver successfully had written 249 bytes to address 0x000D147B
Download minidriver successfully had written 249 bytes to address 0x000D1574
Download minidriver successfully had written 249 bytes to address 0x000D166D
Download minidriver successfully had written 249 bytes to address 0x000D1766
Download minidriver successfully had written 249 bytes to address 0x000D185F
Download minidriver successfully had written 249 bytes to address 0x000D1958
Download minidriver successfully had written 249 bytes to address 0x000D1A51
Download minidriver successfully had written 249 bytes to address 0x000D1B4A
Download minidriver successfully had written 249 bytes to address 0x000D1C43
Download minidriver successfully had written 249 bytes to address 0x000D1D3C
Download minidriver successfully had written 249 bytes to address 0x000D1E35
Download minidriver successfully had written 249 bytes to address 0x000D1F2E
Download minidriver successfully had written 249 bytes to address 0x000D2027
Download minidriver successfully had written 249 bytes to address 0x000D2120
Download minidriver successfully had written 249 bytes to address 0x000D2219
Download minidriver successfully had written 249 bytes to address 0x000D2312
Download minidriver successfully had written 237 bytes to address 0x000D240B
Launch minidriver at 0x000D0200 succeeded
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Terminated with error
Chip erase timeout (nLastProgressReportTime)
Any solution would be really appreciated 😄
Regards
Show Less@Hello.
I review CYW20706 and found that I cannot use i2c and PUART flow control. because puart flow control shares i2c.
Or can you tell me how I can configure it?
I am using a RS232 FTDI adapter to download a hello_sensor_app through the HCI interface. The communication goes fine and the minidriver is launched OK but the log file shows the module memory has a mistmatch in the bytes writen and read.
I append here the last lines of the log:
A total of 2 contiguous memory areas were filled:
[FF000000..FF000027] DATA (40 bytes)
[FF003000..FF01419B] DATA (70044 bytes)
Download config error trying to verify 40 bytes at address 0xFF000000 (SOURCE: CONFIG Configuration data build/hello_sensor-CYBT_343026_EVAL-rom-ram-Wiced-release/hello_sensor-CYBT_343026_EVAL-rom-ram-Wiced-release.hex) (Data mismatch at address 0xFF000000. Expected byte value 0x01 but device contains 0x66)
Please, help.
Thanks,
Show LessI want to wire a CYBT-353027-EVAL to the CODEC MAX 98090 via I2S running the Headset Demo Application.
Try #1: CYBT-353027 is I2S Master
I programmed the Headset app into the BT module and paired it to a cell phone. I wired the I2S to the MAX 98090 Eval Board. I started a music player on the phone. As a consequence, I can hear music in the earphones connected to the MAX 98090. I can also see that there is an I2S BCLK, I2S LRCLK and I2S Data going on using a Logic Analyzer. The LRCLK rate is 48 kHz.
I ended the music player app on the phone an initiated a phone call to another cell phone. The I2S BCLK and I2S LRCLK changed. The LRCLK is now running on 16 kHz. However, there is *nothing* to be seen on the SDIN and SDOUT lines. I disconnected the SDIN and SDOUT lines and, funny enough, there is a signal on the SDOUT line at least.
I assumed, it is pulled to low by the MAX 98090 CODEC.
So I decided to change the roles and make the CODEC the I2S master and the BT module the slave.
Try #2: MAX 98090 is I2S Master
I changed the source code to make the Headset Demo app configure the BT module as I2S Slave and set up the MAX 98090 as I2S master, running the LRCLK at 16 kHz with BCLK set to 64 x fs and an MCLK of 12 MHz.
I checked with the music player app on the phone - it works (although the sound is too loud and clipped).
I tried to make a phone call and again - nothing is on SDIN and SDOUT.
Question: Does this even work?
Which CODEC is recommended to use with the CYBT-353027 to get the I2S working in a bidirectional manner?
Show LessHi,
我想把hci_audio_gateway demo里的hci_ag_cfg_settings里的ble_scan_cfg.high_duty_scan_duration=0设置成永远都在high scan,但是测试下来以后,好像scan了一轮后就不scan了。如下是我的的配置。请帮我确认一下
In our existing project we use CYBT-353027-02 module and WICED Studio 6.4. The CYBT module is running in embedded mode. The module is connected to a host CPU via UART. CYBT firmware update is done via UART, using correspondent minidriver.
Question: after loading minidriver to RAM we execute HCI_FLASH_ERASE command (0x01, 0xCE, 0xFF, 0x04, 0x00, 0x00, 0x00, 0xFF). Is it really necessary? Our goal is to keep application data in CYBT untouched after firmware upgrade, i.e. to keep link keys, BT MAC address and so on. Is it possible?
Show LessHi there. I'd like to know if the CYW20706 can be used directly via HCI H4 (ignoring the WICED Bluetooth stack on the chip) with a full stack on the main MCU, and if yes, how.
In the CYW920706WCDEVAL Evaluation Kit Hardware User Guide, I found this in chapter 9.3:
"In CYW20706, it is available only for application-defined HCI commands and events; it is not for Bluetooth standard HCI commands.
In CYW20706, it is used to communicate with the external MCU and does support Bluetooth standard HCI commands."
The first sentence says it's not possible, while the second one says it is.
The product number is similar to e.g. CYW20710 which did support HCI H4, so I thought it might be an interesting Bluetooth Controller to officially support in our Bluetooth stack. There aren't many new dual-mode chipsets released by other vendors...
Best regards
Matthias Ringwald, BlueKitchen GmbH
Show LessCypress_FOTA_release-v3.1.0 or btsdk-peer-apps-ota-master OtaUpgrade 프로젝트 진행
Cypress PuriCare Mask기기 제품 등록중 file load성공후 Upgrade 버튼 클릭시 "Invalid WICED OFU services" 메세지 발생
otaService, otaControlPoint, otaControlData 모두 nil
var isWicedOfuSeviceValid: Bool {
return otaService != nil && otaControlPoint != nil && otaControlData != nil
}
if !activePeripheral!.isWicedOfuSeviceValid {
self.appendLog("Invalid WICED OFU services")
return
}
해당 값들이 세팅안된 이유를 살펴 보다 보니
peripheral.services 빈배열로 되어있어서 더이상 진행이 안되고 있습니다.
AOS 샘플앱에서는 Cypress 펌웨어 업데이트 성공된 제품입니다.
안되는 이유가 있을까요?
수정된 버전을 받고 싶습니다.
Show LessUser | Count |
---|---|
12 | |
11 | |
4 | |
4 |