Studio Bluetooth Forum Discussions
Hello
Is there a any way to measure Bluetooth error rate or throughput as well as RSSI?
Thanks,
Hello Infineon Support team
[Background]
We are evaluating CYBT-343026-01.
Regarding RF regulatory certifications for Japan, we have referred "MIC_203-JN0721-Cert-i02.pdf" which is attached in the following thread.
https://community.cypress.com/t5/Knowledge-Base-Articles/RF-Regulatory-Certifications-for-CYBT-343026-01-CYBT-343029-01/ta-p/251279
[Question]
To satisfy the regulation of "MIC_203-JN0721-Cert-i02.pdf", please tell us the tx power(in dBm) which we should configure in the application.
Thanks,
Yoshinori
I am looking for an eval kit recommendation which can support a turnkey working demo to a COTS bluetooth headset. I imagine a WICED module is appropriate.
The WICED module should stream an I2S input/output corresponding to the headset speaker/microphone. A simple casted pairing to a fixed headset is only required for a proof-of-concept system which has no OS.
I've worked with Pioneer Kit PSoC 4 modules in the past, but I imagine WICED is the new path.
Long RF range of 250 feet is ideal to ensure a decent link w/ low probabilty of comm loss. Does the below module seem appropriate and what is the best dev kit to be able to break out an I2S link to my custom hardware:
https://www.cypress.com/documentation/datasheets/cybt-3330xx-02-ez-bt-wiced-module
Thanks for any recommendations.
Show Less
Please let me know regarding the maximum clock and maximum bit of I2S for CYBT-343026 WICED 6.6.
The CYW20706 data sheet states on page 39 that the maximum clock is 3.072MHz for slaves.
Considering this in stereo data, 96kHz x 32bit = 3.072MHz (that is, 96kHz Sampling 16bit LR data),
Is it correct to understand that 48kHz x 48bit = 2.304MHz (that is, 48kHz Sampling 24bit LR data) can also be received?
In that case, how should I set it in WICED 6.6?
Hi,
I have a BLE sensor updating its manufacturer data to send the read values. This sensor is non-connectable and I'm trying to setup a CYBT-343026 to read the manuf data of the sensor and update a notify characteristic so the subscribed clients receive the data.
I've been looking for some examples inside the wiced github but weren't able to find anything useful.
Is the proposed solution possible? Or the chip is not able to change between observer and advertise?
Thanks in advance.
Show Less
i have developing the HID device on WICED 6.2 using CYW20706.
and i have testing the connection with HID Host & Client Control App that is provided to example.
but, it does not working well. i want to check the disconnection after supervision timeout that is set to that i want.
is the setting supervision timeout supported in WICED 6.2 on CYW20706?
i knew the supervision timeout can set in role of master, so i was set the role to master before set the supervision timeout.
also, is the process of setting supported?
i need the help. please help me anybody.
thanks.
Show LessI have the CYW20706 BLE board, and I am having trouble debugging using the Segger JLink edu.
On the hardware user guide, it says that I can set up the UART for SWD debugging by plugging the JLink TMS (SWDIO) and the TCK (SWDCK) into the BT_UART_RXD and the BT_UART_TXD respectively.
But when I do this, I still receive this error:
J-Link GDB Server failed:
Could not connect to target. Please check if target is powered and if ribbon cable is plugged properly.
For more details, see the JLinkGDBServerCLExe console.
I plugged in the VTref into the 3.3V supply and GND into ground.
Is there anything else that I need to do to configure the UART? I included the
uart_SetBaudrate(0, 0, 3000000); //and
wiced_set_debug_uart(WICED_ROUTE_DEBUG_TO_HCI_UART );
into the program.
Thank you
Show Lessi have using the API of starting to "BTM_" in WICED tools of 6.2 version.
its loook for working well, but i can't guarantee that.
is the ""BTM_" API support CYW20706 of WICED 6.2 version?
Show Lesshi,
i have found the bonding status of pairing event is changed when device is connecting.
i want to know what is bonding status. it is different with "wiced_result_t"
where the mean of bonding status is in?
i want to know bonding status value it have same with structure as below.
typedef struct {
uint8_t *bd_addr; /**< peer address */
wiced_bt_transport_t transport; /**< BT_TRANSPORT_BR_EDR or BT_TRANSPORT_LE */
wiced_bt_dev_pairing_info_t pairing_complete_info; /**< Transport dependent pairing complete infomation */
wiced_result_t bonding_status; /**< current status of bonding process to notify app of completion status of storing keys */
} wiced_bt_dev_pairing_cplt_t;
thanks.
Show Less