Studio Bluetooth Forum Discussions
Hello,
Following this guide, Cypress BLE Mesh Solution , I can use CYW920719Q40EVB as a provisioner to provision an unprovisioned board and this board has GenericOnOffServer, so I can use "LightControl" tab to control the light on or off.
But now, I have a question that I want to use specific netkey and appkey by myself, how can I configure it?
Thanks,
Kai
Show LessHello,
I don't understand why my program doesn't exit the main loop when an Rx interrupt occurs. It's working when I delete the loop.
This is my program :
#include "wiced.h"
#include "sparcommon.h"
#include "wiced_platform.h"
#include "wiced_rtos.h"
#include "wiced_hal_gpio.h"
#include "wiced_bt_trace.h"
#include "wiced_hal_puart.h"
char data;
void puar_rx_interrupt_callback(void* unused)
{
data = 'b';
}
APPLICATION_START()
{
wiced_hal_puart_init();
wiced_hal_puart_register_interrupt(puar_rx_interrupt_callback);
wiced_hal_puart_set_watermark_level(1);
data='a';
while(1)
{
wiced_hal_puart_write(data);
wiced_rtos_delay_milliseconds(500,KEEP_THREAD_ACTIVE );
}
}
Thank you for your help.
Show LessHello all. I am using cypress 20719-B1 bluetooth development kit and wiced 6.1 SDK. I am using thhe hellosensor example from the sdk. Now I want to flash this hellosensor bin file from the android app. To do this what I have to do please suggest.
Show LessI cant find the below directories in my PC after installing WICED-Studio-6.1 Studio. Strangely this gets installed in the AppData/Local instead of Program files.
This is the exe : WICED-Studio-6.1.0.85-IDE-Installer.exe I have installed.
WICED-Studio-6.1\common\apps\snip\mesh\peerapps\Android\src\bin
and
WICED-Studio-6.1\common\apps\snip\mesh\ClientControl\Release
I am getting the Below snapshot :
Any suggestion.
Sorry since PC GUI tool for Bluetooth Mesh was locked for editing I had to put a different thread. You can delete and reply in the same thread.
Sorry again for this.
Did I installed the wrong installer?
Br,
Pv
Show LessHello All!
I have a question about bt scan( or inquiry),I need to scan for BT beacon continuously and get its rssi information to obtain its roughly location.Is there someAPIS to make it works as expected or change API's arguments to get the same affect?
thanks!
Show LessI'm using CYBT-423028-EVAL-01.
I installed the SDK following the instructions in the package (refer to KBA223637). The WICED studio still have problem resolving symbols. I have both CYBLE920719Q40EVB-01 and CYBT-423028-EVAL-01. It seems the system can not decide which one to use when I compile. The .h files looks very
here's how wiced_platform.h looks like from the first directory:
here's how wiced_platform.h looks like from the second directory.
Except the line number is different, everything else looks the same. From previous posts, it may seem like this isn't an issue for other people. I can't say it's the same for me.
Any idea on how to tell the compiler to use which .h file? otherwise, i'll just have to use GPIO_EN_INT_BOTH_EDGE.
interrupt configs seem to work, but PLATFORM_GPIO_0 through PLATFORM_GPIO_15 are problematic.
Thanks!
Show LessI am using CYBT-343026-EVAL with WICED 6.2 now.
Could you tell me how many BT-Headset can pairing to this module at the same time?
If the number can change,could you tell me where can I change it?shjlaxel.lin_1746341goto-t_2353976user_437857088user_140663973
Show LessHello,
Can you confirm that we can NOT use the ADC Audio Mode with the CYW20719 Dev Kit (CYW920719Q40EVB-01) ?
I guess it is impossible because the dev board is equip with a CYW20719 - 40 QFN package (CYW20719 and CYW20735 Analog to Digital Converter(ADC) ).
Thank you,
Thibaut.
Show LessHello,
is there a PC GUI tool for Bluetooth mesh for Cypress Solution?
I have seen few days back on google and then I couldnt locate it on the site.I think it was a tool to send BleMesh commands over Serial interface to the Device.It has lots of GUI option based on the Mesh SIG spec.
Kindly help !
Br,
Pv
Show LessI am using the CYW20719B1KUMLG Bluetooth dual-mode chip. We were having issues getting the pin P16 to work as a simple GPIO. It turns out we aren’t able to change it to a GPIO. This is a huge issue as we need this pin the work as a GPIO. We need to know if this is a hardware issue or a software issue. I.e. is there no connection to a GPIO in the pinout or does the IDE have limitations on registers it can access so it can’t make P16 a simple GPIO.
Show Less