Studio Bluetooth Forum Discussions
Is there an example project for assigning BLE address? I want the firmware to generate a random static address on first power up and store it in flash to use from then onwards. I tried the 3. option from this post but it does not work. The address I set is not used but a new random address is used every time I reprogram the app.
Configuring the Bluetooth device address in CYW20706
Show LessI am using CYW20719 and I am setting advertising data with wiced_bt_ble_set_raw_advertisement_data() on power up. I can restart advertisement after timeout without problems. If I connect BTSpy to print the WICED_BT_TRACE() logs, it will erase the advertisement data I set and advertise with empty data. Does anyone know why this happens?
Show LessHi,
According to AN91445,there is antenna radiation pattern in P.13.
AN91445: http://www.cypress.com/file/136236/download
Q1: Is PCB antenna of CYBT342036 the same specification?
Q2: How long does the customer need to separate from screw hole?
Thank you.
--TAK
Show LessHI
As we know, the application code is stored in the external memory, how the application code for Cyw20735 start to run after power on? Can I know the boot sequence of Cyw20735?
Show LessI am using CYBT-343026-EVAL with WICED 6.2 now.
At first I use CYBT-343026-EVAL pairs to a BT Headset.It will birth a handle number a.
Then I bring the BT Headset far away that enough to make BT Headset AG disconnected.
After that ,bringing BT Headset back to CYBT-343026-EVAL,It will AG connect again and birth a handle number b,too.
I want to know
1.Whether handle number a and b are the same number?
2.Does handle number b is a num that does not used yet,or use the handle number a because of it's the same BT Headset?
shjluser_437857088goto-t_2353976shjl
Show LessHi,
Looking for a single chip (or module) solution for MCU with Bluetooth/BLE and USB. I need USB to use as Mass Storage once it connected to computer. Except USB I'll need to control number of GPIOs, I2C and SPI.
From other vendors I was suggested for following candidates:
a) nRF52840 by NordicSemi
b) QN9080 by NXP
Please suggest what I can use based on Cypress products.
Regards,
Andrey...
Message was edited by: Andrey Nekhamkin
Show LessDo we have wiced firmware architecture introduce ? if have the simply flow chart will be better.
And which code store in which area, store in ROM or in flash ?
Show Less