Studio Bluetooth Forum Discussions
text.format{('custom.tabs.no.results')}
Hi,
I am using CYW92070xV3_EVAL and WICED studio 6.1,my make target is "snip.mesh.mesh_onoff_server-CYW920706WCDEVAL LEGACY_BOARD=1 download"
But when i use app to add device ,can't scan my 20706.
my log as shown below:
setup nvram ids: net_key_max_num:4 app_key_max_num:8 3c-75
Mesh Start
[Rx]mesh_management_cback: 15
management_cback: LOCAL_IDENTITY_KEYS_REQUEST_EVT: result:0 keys:
mesh_management_cback: 0
***** Free mem before app_init:34684
## mesh_application_init ##
wiced_bt_[Rx]gatt_register: 0
ds1:0x00504000, len:0x0007e000
ds2:0x00582000, len:0x0007e000
platform btp: Config_DS_Location 0x00003000, Confi[Rx]g_VS_Location:0x00001000
WARNING: Upgrade will fail - active DS is not one of the expected locations
WARNING: Are ConfigDSLocation and DLConfigVSLocation in the .btp set up as in nv_loc_len[]?
mesh_application_init: wiced_bt_mesh_core_ota_fw_upgrade_init failed
[Rx]mesh_application_init: unprovisioned GATT DB status:0
***** Free mem after app_init:33156[Rx]
Thanks,
Leo
Show LessCould you tell me that if the initial state including S/W is exactly the same about CYBT - 343026 - 01 below two cases?
1, To be implemented on the evaluation board
2, To be purchased as a reel item
For example, I think that the port setting of PUART of the evaluation board mounted product is as shown in the circuit diagram of the evaluation board.
I would like to check if the reel product setting that it is a difference such as data sheet.
Hello all,
I have designed the custom hardware for the 20719 B1 cypress BLE. When I flash the Hello_sensor demo code. The Bluetooth is not advertising. If flash the same code into the evaluation kit then it is advertising. What could be the issue please suggest me. I have attached the hardware design file to this query. Please find the attached file.
Best Regards,
Rawootray PAtil.
Show LessHi
I want to use part number CYW20719 in my project which requires raspberry pi 3 os. So, is there any software support to interface this controller with raspberry pi 3 possessing raspbian stretch os.
Any help would be great .
Show LessI'd like to confirm how to make WASS application.
Can I get "WICED pro" and related document?
I am trying to program the 20719 devkit using the PSoC 4200L USB devkit and I am having problems. I configured the PSoC4 for USB CDC and connected the UART port to the HCI UART on the 20719. I just forward data between the USB CDC and the UART on the PSoC4. When I start download the app in WICED Studio, I can only get a response from the 20719 if I set the baud rate to 115200. After the minidriver is programmed, the host changes the baud rate to 3000000. I send this command to the 20719 at 115200 but don't receive any response afterwards. The HCI document says the response to this command should be sent back to the host at the original baud rate. When should I be changing baud rates on the PSoC4? I tried to set the baud rate to 3000000 at the beginning of programming but I don't receive any response from the 20719. Does the 20719 support 3000000 in recovery mode?
Show LessCould you provide photo of CYBT-343026-01?
(Photo of the state which isn't mounted)
Hi,
I'm developing an audio application with the CYW920719Q40EVB_01 and Wiced Studio 6.2.
I tried to use the demo/watch example and I modified it as an A2DP source routing with I2S instead UART ( "wiced_audio_start( WICED_TRUE, AUDIO_ROUTE_I2S, lcid, &av_app_cb.sbc_caps_configured );" ). And I use the default configuration of pins , ( platforms/CYW920719Q40EVB_01/wiced_platforme_pin_config.c ) where clock = P16, WS = P17, DO= P02 ans DI=P04. But Clock (pin 16) stay at high level.
I tried to use others pins or configure I2S in slave mode. But they both did not work. The example works well when I'm using uart or sin routing. According to this post, my solution should work https://community.cypress.com/thread/36044?q=I2S
Do you have any clue about that it's working wrong?
Thank you,
Thibaut.
Show LessPlease provide the report of certification acquisition at CYBT-343026-01.
(FCC, ISED, MIC, CE etc)