Studio Bluetooth Forum Discussions
i have test the connection HID Device with my phone. The case of test is as below.
- Chipset & EVK : CYW20706 & F1DC2076 EVB (made in F1media)
- WICED SDK version : WCIED 6.2.1
- Test application : HID Device
and my test condition is as below. it is aging test.
android: power on → inquiry → connect to CYW20706 → connected → 30 seconds idle → reset
CYW20706: power on → paring enable → ready → connected → idle → disconnected → wdog reset
it is disconnected after about 37 test.
i attached log each case of connected normally and disconnected.
anybody help me please.
Show LessBluetooth SIG reports some vulnerabilities ware found.
Could you let me know whether WICED Studio 6.x is affected or not ?
Show Less
I installed WICED Studio v6.6.0.9 on Win10 x64
I only see project folder for \43xxx_Wi-Fi\
I do not see project folder for \20706-A2_Bluetooth\
I am investigating the demos only at this point and I did not plug in any 20706-Based dev kit yet via USB to the PC.
Is this latest WICED Studio version supposed to install the 20706-Based demos? If not, how do I install them... or what version of WICED Studio installs correctly?
Show Less
https://community.cypress.com/message/158986#158986
Then, it is a description that you must use. Is there a problem if SPI2_MOSI remains NoConnect as specified in 343026?
BDR / EDR + 12dBm setting → BDR + 12dBm (typ) / EDR + 9dBm (typ)
BLE + 8dBm setting → BLE + 9dBm (max)
but is it possible to measure the RSSI of the radio wave output
by the command operation with the module of the other party?
Hello
I think 96kHz_16bit Stereo Or When receiving 88.2kHz_16bit Stereo with I2S slave It is not necessary to specify them on WICED, and Sampling Frequency on WICED.
48kHz Or 44.1kHz and Is it okay to understand that the data received by the private internal logic is DownSampled just by specifying it?
Thanks,
Show Less
Hello
I am currently running CYBT-343026 on WICED 6.4.
After that, is it possible to perform an output test as described in ManufacturingBluetoothTestTool only by operating from the host CPU on the product main system without connecting to a PC?