Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Studio Bluetooth Forum Discussions

yapi_4185356
Studio Bluetooth
I would like to know how to use HID and voice mike devices on CYW20735? Show More
juerc_3891021
Studio Bluetooth
Hello,I am trying to send TX and RX data simultaneously as fast as possible. When the RFCOMM buffer is about full, I inform peer to stop sending with ... Show More
YoJa_3107936
Studio Bluetooth
HiCurrently, Customer has encountered a problem that no response was given toRESET_Command before writing FW in Pre-production.They tried 11pcs module... Show More
user_4235866
Studio Bluetooth
Hello,We need to use the RSSI value of BLE signals sent from the Smartphone to estimate the distance between the Smartphone and the Reader Device. Unf... Show More
YaTr_3516311
Studio Bluetooth
Hi,I use CYBT-343026-01 module with ezserial_343026-CYBT_343026_EVAL-rom-ram-Wiced-release FW. I tested it via uart send API command to it. But find t... Show More
YaTr_3516311
Studio Bluetooth
Hi,I want to custome uart protocol to modify advertisement data when uart recieve "SAD,D=0102" command.But once I set "SAD,D=0102" command from uart w... Show More
YaTr_3516311
Studio Bluetooth
Hi,I get CYBT-343026-01 module. I want to download new image to CYBT343026-01 module. I have tested CYBT343026-01 EVAL board and use WICED-Studio tool... Show More
YaTr_3516311
Studio Bluetooth
Hi,I want to use ezserial_343026-CYBT_343026_EVAL-rom-ram-Wiced-release FW in CYBT-343026-01.  Is the hardware design OK for this officail release?UAR... Show More
user_4160961
Studio Bluetooth
Is  CYPRESS planning to release a +10 dBm EIRP (or more)  BT 5 module implementing Coded PHY modulation, in the near future? Thanks Show More
chyac_4036791
Studio Bluetooth
Hi,We are using the 20719 board and we are wondering if it is possible to have an audio input from a bluetooth device and have that audio data transfe... Show More
Forum Information

Studio Bluetooth

Discussion forum regarding WICED Studio Bluetooth topics.