Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

YaTr_3516311
Level 5
Level 5
25 sign-ins First solution authored 100 replies posted

Hi,

I want to test OTA function with CYBT-343026-01 EVAL board. and I do the steps to "Run WsOtaUpgrade.exe ezserial_343026-CYBT_343026_EVAL-rom-ram-Wiced-release.ota.bin.", but when I double click "WsOtaUpgrade.exe", it appears "Fail to open the patch file". I don't why this happen. I have tried two computer with WIN10.

BR,

Treacy

0 Likes
1 Solution

Hi Treacy,

I just tried opening the app in my PC.

You need to open it from the command line.

1. Open the command line from the app folder location

2. Pass the bin file as input

    Refer the screenshot attached

Otaupgrade.png

3. Run it

It should open now.

Thanks,
Anjana

View solution in original post

5 Replies
AnjanaM_61
Moderator
Moderator
Moderator
First comment on KBA 5 questions asked First question asked

Hi Treacy,

Seems like there is some issue with the app. Will escalate the issue to software team.

Will update you.

Thanks,
Anjana

0 Likes

Dear AnjanaM,

When will fix this problem?

BR,

Treacy

0 Likes

Hi Treacy,

I just tried opening the app in my PC.

You need to open it from the command line.

1. Open the command line from the app folder location

2. Pass the bin file as input

    Refer the screenshot attached

Otaupgrade.png

3. Run it

It should open now.

Thanks,
Anjana

Dear AnjanaM,

I tried as your steps, but

1. I can't find the EVAL board BT address in "Select device".

2. What do you mean "Pass the bin file as input", is it iBeacon-CYBT_343026_EVAL-rom-ram-Wiced-release.ota.bin? Then why your screenshot is .elf shown.

pastedImage_0.png

BR,

Treacy

0 Likes

Dear AnjanaM,

I tried >WsOtaUpgrade.exe C:\Users\iBeacon-CYBT_343026-EVAL-rom-ram-Winced-release.ota.bin. It is OK now. Thank you.

0 Likes