Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

NiA_4003596
Level 3
Level 3
First like received Welcome!

Hi,

Could anyone please suggest how to program the module CYBT-483039-02 in modustoolbox 2.1.

What is the platform to be selected to program this module. The available default platforms for CYW20719 in the modustoolbox 2.1 are

pastedImage_2.png

Best regards,

NK

0 Likes
1 Solution
SheetalJ
Moderator
Moderator
Moderator
750 replies posted 500 likes received 500 replies posted

Hi NK,

CYBT-483039-02 is a CYW20719B1 based module, it is not supported in Modus Toolbox. For CYBT-483039-02, you will have to use WICED Studio 6.2 or 6.4 along with platform files WICED Studio: Platform Files for CYBT-483039-EVAL – KBA223747 .

If you are using WICED Studio 6.4, please check Platform and New Patch Files For 20719B1 in WICED 6.4.0.61 - KBA228518

View solution in original post

0 Likes
3 Replies
SheetalJ
Moderator
Moderator
Moderator
750 replies posted 500 likes received 500 replies posted

Hi NK,

CYBT-483039-02 is a CYW20719B1 based module, it is not supported in Modus Toolbox. For CYBT-483039-02, you will have to use WICED Studio 6.2 or 6.4 along with platform files WICED Studio: Platform Files for CYBT-483039-EVAL – KBA223747 .

If you are using WICED Studio 6.4, please check Platform and New Patch Files For 20719B1 in WICED 6.4.0.61 - KBA228518

0 Likes

Hi,

Thank you for the valuable information.

I am using this module for LED lighting application and configured pins for PWM(P28), relay(P26) and on board led indication(P17). Enclosed my schematic for your understanding.

1. How to configure pin P17 as GPIO to light up indication led LED1 because the following code does not work in WICED6.4

     wiced_hal_gpio_configure_pin(WICED_P17, GPIO_OUTPUT_ENABLE, GPIO_PIN_OUTPUT_HIGH);

     wiced_hal_gpio_set_pin_output(WICED_P17, GPIO_PIN_OUTPUT_HIGH);

2. How to configure pin P28 as PWM because the following code does not work in WICED 6.4

    wiced_hal_aclk_enable(PWM_INP_CLK_IN_HZ, ACLK1, ACLK_FREQ_24_MHZ);

    wiced_hal_gpio_select_function(WICED_P28, PWM1);

    // wiced_hal_pwm_configure_pin(WICED_P28, PWM1);

    wiced_hal_pwm_get_params(PWM_INP_CLK_IN_HZ, 0, PWM_FREQ_IN_HZ, &pwm_config);

    wiced_hal_pwm_start(PWM1, PMU_CLK, pwm_config.toggle_count, pwm_config.init_count, 1);

    //set pwm duty cycle

    wiced_hal_pwm_get_params(PWM_INP_CLK_IN_HZ, brightness_level, PWM_FREQ_IN_HZ, &pwm_config);

    wiced_hal_pwm_change_values(PWM1, pwm_config.toggle_count, pwm_config.init_count);

3. I am getting the following PUART message in the terminal with baudrate 115200, could we get meaningful starting message instead of some junk message?

Ý_öûöý[KöÛÚûÉÚ?Ýòù½ÛÚû{¶ýÛÉÛéûÉÛÉkééIserver trans start time:0 target:3490 present:0 state:2648a8

server trans complete:3490

mesh light srv set level element:0 actual/target:15123/3490 linear/target:15123/3490 remaining_time:0

***** Free mem after app_init:142128

Best regards,

NK

0 Likes
SheetalJ
Moderator
Moderator
Moderator
750 replies posted 500 likes received 500 replies posted

Hi NK,

Would you please create a new thread in order to follow your application error issue? It will be easier to track the problem that way.

0 Likes