Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello,

In a hands-free application using BLE communication,

What is an effective way to reduce power consumption?

The power save option is not available in my application.

CYW20706 is the main host, so I can't use the deep sleep mode.

And the application is using a periodic timer(several tens of milliseconds),

so I can't use the low power sleep mode.

Please give me some advice on waht to do.

Thank you!

0 Likes
1 Solution
Anonymous
Not applicable

Hi Aaron,

When you say 'handsfree' are you referring to HFP? What are you using BLE for?

Have you read this article? CYW20706 – BLE Low Power Beacon

You could use the wiced_sleep_config() API to reduce power consumption but if a applicaiton timer is running always, then I don't think there will be any power reduction.

You should be looking at reducing power by changing Tx power or intervals or slave latency (for BLE).

View solution in original post

4 Replies
Anonymous
Not applicable

Hi Aaron,

When you say 'handsfree' are you referring to HFP? What are you using BLE for?

Have you read this article? CYW20706 – BLE Low Power Beacon

You could use the wiced_sleep_config() API to reduce power consumption but if a applicaiton timer is running always, then I don't think there will be any power reduction.

You should be looking at reducing power by changing Tx power or intervals or slave latency (for BLE).

Anonymous
Not applicable

Hi yssu,

Thank you for your reply.

yes, HFP is right.

And BLE uses several services(GATT, Serial GATT, ANCS, etc) to communicate with the smartphone app.

I know the article.

I don't expect to use wiced_sleep_config() API to reduce power consumption,

My application has several periodic timers

So I asked if there was any other way, especially in hfp.

Thank you.

0 Likes
Anonymous
Not applicable

There is nothing much you could do to reduce power consumption in an Audio application such as HFP.

You could maybe reduce the Tx power. Apart from this, I cannot think of any ways to reduce the current consumption.

0 Likes
Anonymous
Not applicable

Thank you, yssu.

0 Likes