Hello!
I want to learn more about using wiced_transport_send_raw_buffer. Stumbled upon her description in wiced_transport.h.
/**
* Function wiced_transport_send_raw_buffer
*
* Used when transport mode is WICED_TRANSPORT_UART_RAW_MODE. Available with the wiced_uart_raw_mode_lib.
* Send the packet to the host over the transport using the buffer allocated by the application.
* This function takes care of preparing the header and sending the data. The buffer must be freed
* by the application if return status is WICED_SUCCESS.
*
* Note: Application has to allocate buffer from transport pool using wiced_transport_allocate_buffer
* and copy the payload to this buffer and send the payload pointer.
* This allows the application to use custom size buffers and avoid overrun of generic buffers,
* which is shared across firmware code.
*
*@param[in] p_buf :Pointer to the payload
*@param[in] length :Payload length
* @return wiced_result_t
*/
wiced_result_t wiced_transport_send_raw_buffer( uint8_t* p_buf, uint16_t length );
When compiling using this function, I got an error - undefined reference to `wiced_transport_send_raw_buffer'.
As far as I understood, I need the wiced_uart_raw_mode_lib library. Where can I get it and how can I connect it?
Thank you!
Solved! Go to Solution.
Hi,
The latest BTSDK (v2.5) does not have the supporting library.
wiced_uart_raw_mode_lib library will be added to the next BTSDK release, hopefully with a sample application.
Thanks,
-Dheeraj
Hi,
May I know which platform (device) are you using?
Thanks,
-Dheeraj
Hi,
The latest BTSDK (v2.5) does not have the supporting library.
wiced_uart_raw_mode_lib library will be added to the next BTSDK release, hopefully with a sample application.
Thanks,
-Dheeraj
Next release should come out in couple of weeks.