Setup a GATT server over BR/EDR

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
mom_4514501
Level 1
Level 1

Hi,

I am using Cypress CYW4343 chipset for a PoC with i.MX6UL-EVK for a Bluetooth application. We are able to create a GATT profile over LE connection using pyBluez and the communication is happening perfectly, but the bottleneck is the speed. For which we are trying to understand if we could utilize the GATT server over EDR as the chipset supports BR/EDR/LE.

In the attached Bluetooth SIG document, we see that optionally the GATT role configuration is possible over BR/EDR.

I am a bit confused about this configuration. Can I get an insight on that, and if this is possible, we would like to use it for our development with CYW4343 or CYW20706.

  

Thanks & Regards

     Aslam

0 Likes
1 Solution
AnjanaM_61
Moderator
Moderator
Moderator
10 questions asked 5 comments on KBA First comment on KBA

Hi ,

As per BT spec, there is an option for opening GATT over BR/EDR connection. In WICED , we have the API wiced_bt_gatt_bredr_connect .

In that case, wiced_bt_transport_t  of wiced_bt_gatt_connection_status_t  should result in BT_TRANSPORT_BR_EDR

As per my knowledge this is not used in any profiles currently. So this option can't be used for current applications.

Reference: https://epxx.co/artigos/bluetooth_gatt.html

Thanks,

Anjana

View solution in original post

0 Likes
1 Reply
AnjanaM_61
Moderator
Moderator
Moderator
10 questions asked 5 comments on KBA First comment on KBA

Hi ,

As per BT spec, there is an option for opening GATT over BR/EDR connection. In WICED , we have the API wiced_bt_gatt_bredr_connect .

In that case, wiced_bt_transport_t  of wiced_bt_gatt_connection_status_t  should result in BT_TRANSPORT_BR_EDR

As per my knowledge this is not used in any profiles currently. So this option can't be used for current applications.

Reference: https://epxx.co/artigos/bluetooth_gatt.html

Thanks,

Anjana

0 Likes