Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
NiLi_2861801
Level 3
Level 3
First like received First like given

Hi,

      I followed the example : 20719-B1_Bluetooth\apps\snip\hal\spi_master to create a SPI communication with a 3-axis g-sensor. But I found the SPI_CS will back to inactive too early that will cause an incorrect Writing operation. .

      I also used PSOC6 to do the same thing, and PSOC6 did very well:

cs compare.jpg

  

These r the codes:

void init_spi()

{

    wiced_hal_pspi_init(SPI_MASTER, INPUT_PIN_PULL_DOWN, MASTER_P38_CLK_P28_MOSI_P01_MISO, DEFAULT_FREQUENCY, SPI_MSB_FIRST, SPI_SS_ACTIVE_LOW, SPI_MODE_3, SPI_CS);

}

void send_data(unsigned char register_address, unsigned char *value, unsigned char number_of_bytes)

{

  unsigned char send_data[2];

  unsigned char rec_data[8];

  if( 1!= number_of_bytes )
  {
    WICED_BT_TRACE("mcube_read_regs bytes error =%d\r\n", number_of_bytes);
  }

  WICED_BT_TRACE("WR: reg = 0x%02x, value = 0x%02x\r\n", register_address, *value);
  send_data[0] = register_address |0x40; // 1 bytes;  write operation
  send_data[1] = *value;

  wiced_hal_pspi_exchange_data(sizeof(send_data), send_data, rec_data);

}

Another question is, Since the SPI_CS is controlled by SPI driver automatically, why the sample code write there red codes?

....

    wiced_hal_gpio_configure_pin(CS, GPIO_OUTPUT_ENABLE, GPIO_PIN_OUTPUT_HIGH);

    wiced_hal_pspi_init(SPI_MASTER, INPUT_PIN_PULL_UP, MASTER_P38_CLK_P28_MOSI_P01_MISO, DEFAULT_FREQUENCY, SPI_LSB_FIRST, SPI_SS_ACTIVE_LOW, SPI_MODE_0, CS);

....

        wiced_hal_gpio_set_pin_output(CS, GPIO_PIN_OUTPUT_LOW);

        wiced_hal_pspi_tx_data(sizeof(start_byte), &start_byte);

        wiced_hal_gpio_set_pin_output(CS, GPIO_PIN_OUTPUT_HIGH);

.....

        wiced_rtos_delay_milliseconds(20, 1);
        wiced_hal_gpio_set_pin_output(CS, GPIO_PIN_OUTPUT_LOW);
        wiced_hal_pspi_rx_data(sizeof(rec_byte), rec_byte);
        wiced_hal_gpio_set_pin_output(CS, GPIO_PIN_OUTPUT_HIGH);

....

0 Likes
1 Solution

linzh_2861801

This was an internal API. WICED 6.2 has replaced this API with wiced_hal_i2c_combined_read. Update your WICED to the latest version and you will be able to see this new API

View solution in original post

7 Replies
Owen_Zhang123
Moderator
Moderator
Moderator
5 questions asked 500 solutions authored 250 sign-ins

Hi,

The cs pin is controlled as GPIO, you can just try to add some delay before you set the cs pin to high state.

0 Likes

Hi zhxh,

    CS is not a GPIO,

    1. After the PIN configured to SPI_CS,  the CS cannot be controlled by  wiced_hal_gpio_set_pin_output(CS, GPIO_PIN_OUTPUT_LOW);

const wiced_platform_gpio_t platform_gpio_pins[] =

    {

        [PLATFORM_GPIO_0 ] = {WICED_P00, WICED_GPIO              },      //Button

        [PLATFORM_GPIO_1 ] = {WICED_P01, WICED_SPI_1_MISO        },

        [PLATFORM_GPIO_2 ] = {WICED_P02, WICED_PCM_OUT_I2S_DO    },

        [PLATFORM_GPIO_3 ] = {WICED_P04, WICED_PCM_IN_I2S_DI    },

        [PLATFORM_GPIO_4 ] = {WICED_P06, WICED_GPIO              },

        [PLATFORM_GPIO_5 ] = {WICED_P07, WICED_SPI_1_CS          },

.....

  wiced_hal_pspi_init(SPI_MASTER, INPUT_PIN_PULL_DOWN, MASTER_P38_CLK_P28_MOSI_P01_MISO, DEFAULT_FREQUENCY, SPI_MSB_FIRST, SPI_SS_ACTIVE_LOW, SPI_MODE_3, SPI_CS);

        MUST:

        wiced_hal_gpio_select_function(SPI_CS, WICED_GPIO),

            wiced_hal_gpio_configure_pin(SPI_CS, GPIO_OUTPUT_ENABLE, GPIO_PIN_OUTPUT_HIGH);

      then you can set pin (SPI_CS).

  2. The SPI_CS will go HIGH /LOW automatically while writing or reading operation even if you comment out these code:

        wiced_hal_gpio_configure_pin(SPI_CS, GPIO_OUTPUT_ENABLE, GPIO_PIN_OUTPUT_HIGH);

        wiced_hal_gpio_set_pin_output(CS, GPIO_PIN_OUTPUT_LOW);

        wiced_hal_gpio_set_pin_output(CS, GPIO_PIN_OUTPUT_HIGH);

0 Likes

ranm

Could you take a look at this please?

0 Likes

Hi,

You need to edit the /20719-B1_Bluetooth/platforms/CYW920719Q40EVB_01/wiced_platform_pin_config.c file as follows (Highlighted text)

Current code:

const wiced_platform_gpio_t platform_gpio_pins[] =

    {

        [PLATFORM_GPIO_0 ] = {WICED_P00, WICED_GPIO              },      //Button

        [PLATFORM_GPIO_1 ] = {WICED_P01, WICED_SPI_1_MISO        },

        [PLATFORM_GPIO_2 ] = {WICED_P02, WICED_PCM_OUT_I2S_DO    },

        [PLATFORM_GPIO_3 ] = {WICED_P04, WICED_PCM_IN_I2S_DI    },

        [PLATFORM_GPIO_4 ] = {WICED_P06, WICED_GCI_GPIO_06      },

        [PLATFORM_GPIO_5 ] = {WICED_P07, WICED_SPI_1_CS          },

        [PLATFORM_GPIO_6 ] = {WICED_P10, WICED_GCI_GPIO_07      },

        [PLATFORM_GPIO_7 ] = {WICED_P16, WICED_PCM_CLK_I2S_CLK  },

        [PLATFORM_GPIO_8 ] = {WICED_P17, WICED_PCM_SYNC_I2S_WS  },

        [PLATFORM_GPIO_9 ] = {WICED_P26, WICED_GPIO              },      //Default LED 2

        [PLATFORM_GPIO_10] = {WICED_P25, WICED_I2C_1_SCL        },

        [PLATFORM_GPIO_11] = {WICED_P28, WICED_SPI_1_MOSI        },      //Optional LED 1

        [PLATFORM_GPIO_12] = {WICED_P29, WICED_I2C_1_SDA        },

        [PLATFORM_GPIO_13] = {WICED_P33, WICED_UART_2_TXD        },

        [PLATFORM_GPIO_14] = {WICED_P34, WICED_UART_2_RXD        },

        [PLATFORM_GPIO_15] = {WICED_P38, WICED_SPI_1_CLK        },

    };

New Code:

const wiced_platform_gpio_t platform_gpio_pins[] =

    {

        [PLATFORM_GPIO_0 ] = {WICED_P00, WICED_GPIO              },      //Button

        [PLATFORM_GPIO_1 ] = {WICED_P01, WICED_SPI_1_MISO        },

        [PLATFORM_GPIO_2 ] = {WICED_P02, WICED_PCM_OUT_I2S_DO    },

        [PLATFORM_GPIO_3 ] = {WICED_P04, WICED_PCM_IN_I2S_DI    },

        [PLATFORM_GPIO_4 ] = {WICED_P06, WICED_GCI_GPIO_06      },

        [PLATFORM_GPIO_5 ] = {WICED_P07, WICED_GPIO         },

        [PLATFORM_GPIO_6 ] = {WICED_P10, WICED_GCI_GPIO_07      },

        [PLATFORM_GPIO_7 ] = {WICED_P16, WICED_PCM_CLK_I2S_CLK  },

        [PLATFORM_GPIO_8 ] = {WICED_P17, WICED_PCM_SYNC_I2S_WS  },

        [PLATFORM_GPIO_9 ] = {WICED_P26, WICED_GPIO              },      //Default LED 2

        [PLATFORM_GPIO_10] = {WICED_P25, WICED_I2C_1_SCL        },

        [PLATFORM_GPIO_11] = {WICED_P28, WICED_SPI_1_MOSI        },      //Optional LED 1

        [PLATFORM_GPIO_12] = {WICED_P29, WICED_I2C_1_SDA        },

        [PLATFORM_GPIO_13] = {WICED_P33, WICED_UART_2_TXD        },

        [PLATFORM_GPIO_14] = {WICED_P34, WICED_UART_2_RXD        },

        [PLATFORM_GPIO_15] = {WICED_P38, WICED_SPI_1_CLK        },

    };

Then you can control the CS pin in your application.

This configuration should be used while using SPI as a master. When using SPI as a slave the CS pin should be connected to the SPI block (like in the default code)

Thanks

Abhishek

0 Likes

Hi amka,

     Yes,  I can change SPI_CS to GPIO use   gpio_select_function, config_pin, and then set_ouput also .

     But writing operation still not work as expected.

     I have to set pins(MOSI/MISO/CLK/CS) to GPIO_SIMULATOR while writing, and it works!.

0 Likes

May I ask I2C question here ?

in the sample code, I2C_MASTER.c :

    i2cm_init();

    if((i2cm_comboRead((UINT8 *)&data, sizeof(UINT8), &reg_add, sizeof(UINT8), LSM9DS1_ACC_GYRO_I2C_ADDRESS)))

I cannot find these two functions Definition or Prototype. But it can compile and running well.

My question is , how to write ?

0 Likes

linzh_2861801

This was an internal API. WICED 6.2 has replaced this API with wiced_hal_i2c_combined_read. Update your WICED to the latest version and you will be able to see this new API