Hi,
I built the "serial gatt service" like this "demo.hci_serial_gatt_service-CYBT_343026_EVAL download DIRECT_LOAD=1 build"
Then download to the CYBT343026 board using "Wiced client control".
It has shown "Launch RAM". However, it still advertises as the previous demo "hello". This new demo application is not working.
Does it need extra downloading?
Thanks
Solved! Go to Solution.
I have found the problem. the boot sequence will not start the application in the RAM if there is one already in the Flash memory.
I have found the problem. the boot sequence will not start the application in the RAM if there is one already in the Flash memory.
Hi JiYa_3557771 ,
DIRECT_LOAD is for RAM download. Which means the application will not be copied to flash. Thus , if you reset after Launch RAM message , application will run from flash . In your case the previously loaded project which is available in flash.
Thanks,
Anjana
Yes, you are correct.
Regards,
Anjana