cancel
Showing results for 
Search instead for 
Did you mean: 

Studio Bluetooth

EdCh_3241771
New Contributor

Hi,

I am development the test code for  CYW20704UA2KFFB1G, there is a  external SPI flash memory, MX25L2006EM1L-12G(2M), connected to the chip via D7,D8,E7,E8 pins.

How can I initialize the flash memory and do the read/write function by HCI command using the UART interface ?

I am using the Bluez 5, is there any example or document I can take reference?

Can I develop the test code based on bluez  or I must use the BSA package to access/program the SPI interface on CYW20704?

Thanks for your help.

0 Likes
1 Solution
BoonT_56
Employee

20704 is currently not supported in this forum. You may have to revert to the Taiwan team that enable you on this.

View solution in original post

1 Reply
BoonT_56
Employee

20704 is currently not supported in this forum. You may have to revert to the Taiwan team that enable you on this.

View solution in original post