Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

JeRi_3276026
Level 1
Level 1
First like given

Please can you explain the Hardwaruser-guide code

BSC-i2c

/*code*/

include wiced_hal_i2c.h.

#define I2C_SLAVE_ADDRESS (0x76)

#define I2C_SLAVE_OPERATION_READ 0

#define I2C_SLAVE_OPERATION_WRITE 1

void test_i2c_driver( void )

{

/*What does it mean ="123456" ¿number bytes?*/

uint8_t data_array[] = "123456";

wiced_hal_i2c_init(WICED_I2C_SDA_P35_SCL_P37);

wiced_hal_i2c_get_speed( );

wiced_hal_i2c_set_speed( I2CM_SPEED_100KHZ );

wiced_hal_i2c_write( data_array, sizeof( data_array ), I2C_SLAVE_ADDRESS);

wiced_hal_i2c_read( data_array, sizeof( data_array ), I2C_SLAVE_ADDRESS);

WICED_BT_TRACE( "Read bytes %s\n\r", data_array );

it does not work

Please Help.

Thanks you team

0 Likes
1 Solution

Please try the attached code. Use the following API to set the I2C speed.

bsc_SetSpeed(BSC_CTL_SCL_xxxKHZ);

wiced_hal_i2c_set_speed(I2CM_SPEED_xxxKHZ);

View solution in original post

4 Replies
JeRi_3276026
Level 1
Level 1
First like given

Route->20706-A2_Bluetooth->apps-snip->hal->i2c_master

Files:

i2c_master.c

makefile.mk

File->makefile.mk

APP_SRC +=i2c_master.c

C_FLAGS += -DWICED_BT_TRACE_ENABLE

File->i2c_master.c

//Include Library\\

#include "wiced_bt_trace.h"

#include "wiced_hal_i2c.h"

//Define Variables\\

/***************************************************************************************

*I2C_SLAVE_ADDRESS REGISTRO 0X76 BMP238

*I2C_SLAVE_OPERATION_READ  0  // DEFINICION DE LECTURA EN 0

*I2C_SLAVE_OPERATION_WRITE 1  // DEFINICION DE ESCRITURA EN 1

****************************************************************************************/

#define I2C_SLAVE_ADDRESS (0x76)

#define I2C_SLAVE_OPERATION_READ 0

#define I2C_SLAVE_OPERATION_WRITE 1

void i2c_master (void)

{

uint8_t data_array[] ="123456";

wiced_hal_i2c_init( WICED_I2C_SDA_P35_SCL_P37 );

    UINT8 I2CM_SPEED_400KHZ;

wiced_hal_i2c_set_speed(I2CM_SPEED_400KHZ);

wiced_hal_i2c_get_speed ();

wiced_hal_i2c_write ( data_array , sizeof ( data_array ), I2C_SLAVE_ADDRESS );

wiced_hal_i2c_read  ( data_array , sizeof ( data_array ), I2C_SLAVE_ADDRESS );

WICED_BT_TRACE ("Read Bytes %\n\r" , data_array );

}

NAME MAKE TARGET

snip.hal.i2c_master-CYW920706WCDEVAL download  UART=COM10  VERBOSE=1

Error:

C:\Users\*\Documents\WICED-Studio-6.2\20706-A2_Bluetooth\Wiced-BT\spar/common/sparinit.c:82: undefined reference to `wiced_bt_app_start'

makefile:300: recipe for target '../../build/i2c_master-CYW920706WCDEVAL-rom-ram-Wiced-release/A_20703A2-i2c_master-rom-ram-spar.elf' failed

make.exe[1]: *** [../../build/i2c_master-CYW920706WCDEVAL-rom-ram-Wiced-release/A_20703A2-i2c_master-rom-ram-spar.elf] Error 1

make.exe[1]: Leaving directory 'C:/Users/*/Documents/WICED-Studio-6.2/20706-A2_Bluetooth/Wiced-BT/spar'

Makefile:536: recipe for target 'snip.hal.i2c_master-CYW920706WCDEVAL' failed

make: *** [snip.hal.i2c_master-CYW920706WCDEVAL] Error 2

0 Likes

Please try the attached code. Use the following API to set the I2C speed.

bsc_SetSpeed(BSC_CTL_SCL_xxxKHZ);

wiced_hal_i2c_set_speed(I2CM_SPEED_xxxKHZ);

Please can you explain.

I don't understand you

You can detail what you want me to do.

//Include Library

#include "wiced_bt_trace.h"

#include "wiced_hal_i2c.h"

//Define Variables

/*

*I2C_SLAVE_ADDRESS REGISTRO 0X76 BMP238

*I2C_SLAVE_OPERATION_READ  0  // DEFINICION DE LECTURA EN 0

*I2C_SLAVE_OPERATION_WRITE 1  // DEFINICION DE ESCRITURA EN 1

*/

#define I2C_SLAVE_ADDRESS (0x76)

#define I2C_SLAVE_OPERATION_READ 0

#define I2C_SLAVE_OPERATION_WRITE 1

void i2c_master (void)

{

uint8_t data_array[] ="123456";

wiced_hal_i2c_init( WICED_I2C_SDA_P35_SCL_P37 );

    UINT8 I2CM_SPEED_100KHZ;

wiced_hal_i2c_set_speed( I2CM_SPEED_100KHZ );

wiced_hal_i2c_get_speed ();

wiced_hal_i2c_write ( data_array , sizeof ( data_array ), I2C_SLAVE_ADDRESS );

wiced_hal_i2c_read  ( data_array , sizeof ( data_array ), I2C_SLAVE_ADDRESS );

WICED_BT_TRACE ("Read Bytes %\n\r" , data_array );

}

Not error the code

Errors:

C:\Users\Zener\Documents\WICED-Studio-6.2\20706-A2_Bluetooth\Wiced-BT\spar/common/sparinit.c:82: undefined reference to `wiced_bt_app_start'

makefile:300: recipe for target '../../build/i2c_master-CYW920706WCDEVAL-rom-ram-Wiced-release/A_20703A2-i2c_master-rom-ram-spar.elf' failed

make.exe[1]: *** [../../build/i2c_master-CYW920706WCDEVAL-rom-ram-Wiced-release/A_20703A2-i2c_master-rom-ram-spar.elf] Error 1

make.exe[1]: Leaving directory 'C:/Users/Zener/Documents/WICED-Studio-6.2/20706-A2_Bluetooth/Wiced-BT/spar'

make: *** [snip.hal.i2c_master-CYW920706WCDEVAL] Error 2

Makefile:536: recipe for target 'snip.hal.i2c_master-CYW920706WCDEVAL' failed

0 Likes

Please unzip the project to your Wiecd SDK file such as: C:\Users\zhxh\Documents\WICED-Studio-6.2.1.2\20706-A2_Bluetooth\apps\demo

And then create a make target, program your kit board.