Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

We have the CYBT-343026-EVAL evaluation board and I am trying to program the SPI flash internal to the module using the UART interface from my custom software.  The document "WICED-HCI-Control-Protocol.pdf" in section 2.5 has some information about how to download into the serial flash but does not have details about the minidriver.  When I look at the download log generated by using the download feature of the Wiced Studio 6.0,  ChipLoad first downloads a UART minidriver and then sends a WICED flash erase command before downloading the application *.HEX file.

Do I need to follow the method of ChipLoad to download the UART minidriver and erase the SPI flash before downloading a *.HEX file?

The source code for client_control is available but this example only downloads a direct *.HCD image.  Is the source code available from ChipLoad showing how to load a *.HEX file to SPI flash?

0 Likes
1 Solution
Anonymous
Not applicable

The sequence we described in the previous reply works on the Cypress CYW920706WCDEVAL Evaluation Kit but not with the CYBT-343026-EVAL evaluation board.  For the CYW920706WCDEVAL eval board we did not have to download the Mini-Driver but for the CYBT-343026-01 module we found we had to download the Mini-Driver.  The Mini-Driver file for the CYBT-343026-01 module can be found in the Wiced Studio folder "Wiced-Studio-6.1\20706-A2_Bluetooth\platforms\CYBT_343026_EVAL\uart.hex" after you install the CYBT-343026-01 platform files.

We are currently using the following steps to program the CYBT-343026-01.  These steps are described in the document "WICED-HCI-Control-Protocol.pdf" section 2.5. 

Setup the CYBT-343026-01 module in code download mode

1) Host computer sets UART_CTS inactive (high) and sets baud rate = 115200

2) Host computer drives signal SPI2_MOSI driven low (we added a FET in parallel with SW2 to drive this signal low)

3) Pulse XRES low then high

4) Disable the FET signal driving SPI2_MOSI  low

The host computer then sends the following command:

1) HCI_RESET: 01 03 0C 00

2) DOWNLOAD_MINIDRIVER: 01 2E FC 00

3) Parse uart.hex and send WRITE_RAM: 01 4C FC nn xx xx xx xx yy yy yy yy ....

4) LAUNCH_RAM to Address 0x000D0200: 01 4E FC 04 00 02 0D 00

where 0x000D0200 is the first download address in the uart.hex file

5) CHIP_ERASE: 01 CE FF 04 00 00 00 FF

6) Parse wiced_app.hex file and send WRITE_RAM: 01 4C FC nn xx xx xx xx yy yy yy yy ....

7) LAUNCH_RAM to Address 0x00000000: 01 4E FC 04 00 00 00 00

View solution in original post

2 Replies
Anonymous
Not applicable

We were able to successfully program a *.HEX file the SPI flash over the UART interface without loading the UART minidriver using the follow commands:

1) HCI_RESET: 01 03 0C 00

2) DOWNLOAD_MINIDRIVER: 01 2E FC 00

3) CHIP_ERASE: 01 CE FF 04 00 00 00 FF

4) Parse *.HEX file and send WRITE_RAM: 01 4C FC nn xx xx xx xx yy yy yy yy ....

5) LAUNCH_RAM to Address 0x00000000: 01 4E FC 04 00 00 00 00

0 Likes
Anonymous
Not applicable

The sequence we described in the previous reply works on the Cypress CYW920706WCDEVAL Evaluation Kit but not with the CYBT-343026-EVAL evaluation board.  For the CYW920706WCDEVAL eval board we did not have to download the Mini-Driver but for the CYBT-343026-01 module we found we had to download the Mini-Driver.  The Mini-Driver file for the CYBT-343026-01 module can be found in the Wiced Studio folder "Wiced-Studio-6.1\20706-A2_Bluetooth\platforms\CYBT_343026_EVAL\uart.hex" after you install the CYBT-343026-01 platform files.

We are currently using the following steps to program the CYBT-343026-01.  These steps are described in the document "WICED-HCI-Control-Protocol.pdf" section 2.5. 

Setup the CYBT-343026-01 module in code download mode

1) Host computer sets UART_CTS inactive (high) and sets baud rate = 115200

2) Host computer drives signal SPI2_MOSI driven low (we added a FET in parallel with SW2 to drive this signal low)

3) Pulse XRES low then high

4) Disable the FET signal driving SPI2_MOSI  low

The host computer then sends the following command:

1) HCI_RESET: 01 03 0C 00

2) DOWNLOAD_MINIDRIVER: 01 2E FC 00

3) Parse uart.hex and send WRITE_RAM: 01 4C FC nn xx xx xx xx yy yy yy yy ....

4) LAUNCH_RAM to Address 0x000D0200: 01 4E FC 04 00 02 0D 00

where 0x000D0200 is the first download address in the uart.hex file

5) CHIP_ERASE: 01 CE FF 04 00 00 00 FF

6) Parse wiced_app.hex file and send WRITE_RAM: 01 4C FC nn xx xx xx xx yy yy yy yy ....

7) LAUNCH_RAM to Address 0x00000000: 01 4E FC 04 00 00 00 00