Programming CYBT-333047-02

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
KeTa_1341526
Level 5
Level 5
Distributor - TED (Japan)
10 likes given 10 likes received 5 likes given

Hello,

F/W is programming to CYBT-333047-02 mounted on the board as shown in the following thread, but Erace ends without completing.

Programming an EZ-BT WICED Module – KBA223428

I have multiple boards, but I can't program about 3 boards.

What do you think is the problem?

[Command]

ChipLoad -BLUETOOLMODE -REBAUDRATE 115200 -LAUNCHADDRESS 0x00000000 -PORT COM5 -BAUDRATE AUTO -MINIDRIVER uart.hex -BTP CYBT_333032_EVAL_SFLASH.btp -CONFIG ezserial_343026-CYBT_343026_EVAL-rom-ram-Wiced-release.hex

* uart.hex and CYBT_333032_EVAL_SFLASH.btp : From  Platform Files for CYBT-333032-EVAL - KBA226800

* ezserial_343026-CYBT_343026_EVAL-rom-ram-Wiced-release.hex: From https://www.cypress.com/documentation/software-and-drivers/ez-serial-ez-ble-module-firmware-platform

[Log]

Trying baudrate 115200   Conn: PORT=COM5    BAUDRATE=115200

Autodetected baudrate 115200

Baudrate change not needed -- already at 115200 baud

Download minidriver successfully had written 249 bytes to address 0x000D0200

Download minidriver successfully had written 249 bytes to address 0x000D02F9

Download minidriver successfully had written 249 bytes to address 0x000D03F2

Download minidriver successfully had written 249 bytes to address 0x000D04EB

Download minidriver successfully had written 249 bytes to address 0x000D05E4

Download minidriver successfully had written 249 bytes to address 0x000D06DD

Download minidriver successfully had written 249 bytes to address 0x000D07D6

Download minidriver successfully had written 249 bytes to address 0x000D08CF

Download minidriver successfully had written 249 bytes to address 0x000D09C8

Download minidriver successfully had written 249 bytes to address 0x000D0AC1

Download minidriver successfully had written 249 bytes to address 0x000D0BBA

Download minidriver successfully had written 249 bytes to address 0x000D0CB3

Download minidriver successfully had written 249 bytes to address 0x000D0DAC

Download minidriver successfully had written 249 bytes to address 0x000D0EA5

Download minidriver successfully had written 249 bytes to address 0x000D0F9E

Download minidriver successfully had written 249 bytes to address 0x000D1097

Download minidriver successfully had written 249 bytes to address 0x000D1190

Download minidriver successfully had written 249 bytes to address 0x000D1289

Download minidriver successfully had written 249 bytes to address 0x000D1382

Download minidriver successfully had written 249 bytes to address 0x000D147B

Download minidriver successfully had written 249 bytes to address 0x000D1574

Download minidriver successfully had written 249 bytes to address 0x000D166D

Download minidriver successfully had written 249 bytes to address 0x000D1766

Download minidriver successfully had written 249 bytes to address 0x000D185F

Download minidriver successfully had written 249 bytes to address 0x000D1958

Download minidriver successfully had written 249 bytes to address 0x000D1A51

Download minidriver successfully had written 249 bytes to address 0x000D1B4A

Download minidriver successfully had written 249 bytes to address 0x000D1C43

Download minidriver successfully had written 249 bytes to address 0x000D1D3C

Download minidriver successfully had written 249 bytes to address 0x000D1E35

Download minidriver successfully had written 249 bytes to address 0x000D1F2E

Download minidriver successfully had written 249 bytes to address 0x000D2027

Download minidriver successfully had written 249 bytes to address 0x000D2120

Download minidriver successfully had written 249 bytes to address 0x000D2219

Download minidriver successfully had written 249 bytes to address 0x000D2312

Download minidriver successfully had written 237 bytes to address 0x000D240B

Launch minidriver at 0x000D0200 succeeded

Transmitting "Chip erase" command   01 CE FF 04 00 00 00 FF

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Executing -- erasing chip

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Terminated with error

Chip erase timeout (nLastProgressReportTime)

Best regards,

Takahashi

0 Likes
1 Solution

The recover mode is operated as follows:

1. Pull Recover(SPI2_MOSI) Pin to GND

2. Pull Reset Pin to GND

3. Release the Reset Pin

4. Release the Recover Pin

Then program the module with the module programmer tool with 115200 baudrate. Could you check the above steps and try again?

View solution in original post

0 Likes
3 Replies