I followed all the instructions from Unable to open wmbt/mbt.exe and it still doesn't work. What is the problem? I get this:
MBT_TRANSPORT: COM42
DOWNLOAD_BAUDRATE: 115200 (default)
APPLICATION_BAUDRATE: 115200 (default)
Sending HCI Command:
0000 < 03 0C 00 >
Received HCI Event:
0000 < 0A >
Failed execute_reset
If I put into recovery mode, reset works once and everything fails after that.
Solved! Go to Solution.
I can send mbt command with remove the "wiced_set_debug_uart( WICED_ROUTE_DEBUG_TO_PUART );" successfully. After download the application with HCI baudrate 115200, please plug out the kit from your computer and plug in again. Then I can send the mbt command.
For the download command, I also have the same problem as you. I recommend you to use the command line method to program the device if you don't want to use the SDK.
Please refer to part 2 of the following KBA "Programming using the command line" about how to program with command line. It is for the module product and also useful for chip.
I got it to work after removing this from the makefile:
C_FLAGS += -DWICED_BT_TRACE_ENABLE
Why do I need to do this when other people got it working without this change? Also I never got an answer from support why debug trace never worked when I set it to use PUART or HCI_UART. I have to use WICED_UART and BTSpy. I open the COM port under putty and see nothing. Is there some problem with my Windows or driver setup?
Are you using the 20719Q40 kit board for your test? Please try to programm an application with HCI UART baudrate set to 115200 and try the mbt tool again.
I am using that board at 115200 and it only works if I remove this line from the hello_sensor test project:
wiced_set_debug_uart( WICED_ROUTE_DEBUG_TO_PUART );
I don't understand why PUART will interfere with HCI UART. Also, does the app download function work with mbt? I tried and it gives an error at the end and hangs at the last HCI reset. The app does not run when I do power reset.
sending record at:0xffffffff
Sending HCI Command:
0000 < 4C FC 04 FF FF FF FF >
Received HCI Event:
0000 < 0E 04 01 4C FC 00 >
Success
Download .hcd file success
Sending HCI Command:
0000 < 4E FC 04 FF FF FF FF >
Received HCI Event:
0000 < 0E 04 01 4E FC 12 >
Failed SendLaunchRam
Failed to send launch RAM
Launch RAM success
Issue HCI Reset after downloading Application
Sending HCI Command:
0000 < 03 0C 00 >
I can send mbt command with remove the "wiced_set_debug_uart( WICED_ROUTE_DEBUG_TO_PUART );" successfully. After download the application with HCI baudrate 115200, please plug out the kit from your computer and plug in again. Then I can send the mbt command.
For the download command, I also have the same problem as you. I recommend you to use the command line method to program the device if you don't want to use the SDK.
Please refer to part 2 of the following KBA "Programming using the command line" about how to program with command line. It is for the module product and also useful for chip.