Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

NiLi_2861801
Level 3
Level 3
First like received First like given

Hi, 

     The sample WICED-Studio-6.2-SDK\common\apps\demo\low_power_sensor,  10s timer will lead the board into SDS mode.  I connect a Ammeter  between PIN2 & PIN4 at jumper J8 and detect current = 0mA while SDS mode. When I press the button(SW3), or connect A5(WICED_P17) to 3.3V,  the board will go a WARM BOOT.

      Then, base on this sample, I modified the file low_power_mode.c (attachment file).  The Ammeter display 0.04mA. and button or P17 will just output a string displaying the event happend, not a boot flow. It seems that the board did not go into SDS.  What did I miss for the sleep configure or other things?

      (What I modified are: delete all the codes about bluetooth, just left the 10S timer and sleep configuration.)

      here are the output:

[2018-06-11_14:32:28]sleep_mode=0

[2018-06-11_14:32:28]Hello Sensor cold Start

[2018-06-11_14:32:28]hello_sensor_application_init

[2018-06-11_14:32:28]idle timer start successful

[2018-06-11_14:32:28]......................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................hello sensor idle.   

[2018-06-11_14:32:38].$.$.@.$.$.@.$.$.@

[2018-06-11_14:35:28].$.$.@hello_sensor_interrupt_handler

[2018-06-11_14:35:34].$.$.@

red line display a button press event.

0 Likes
1 Solution
Anonymous
Not applicable

It is necessary to initialize the stack for the device to enter SDS. If the stack is not initialized, the device enters PDS and not SDS.

So, just add a wiced_bt_stack_init in your application and move the call to hello_sensor_application_init() to BTM_ENABLED_EVT in the management callback. That should solve your problem.

View solution in original post

1 Reply
Anonymous
Not applicable

It is necessary to initialize the stack for the device to enter SDS. If the stack is not initialized, the device enters PDS and not SDS.

So, just add a wiced_bt_stack_init in your application and move the call to hello_sensor_application_init() to BTM_ENABLED_EVT in the management callback. That should solve your problem.