Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

MiRo_263836
Level 5
Level 5
100 replies posted 50 likes received 50 replies posted

I am targeting the CYW20719

0 Likes
1 Solution

Take a look at /20706-A2_Bluetooth/apps/snip/bt/hci_handsfree

* Features demonstrated

*  - WICED BT Handsfree (Device) APIs

*  - Handling of the UART WICED protocol

*  - SDP configuration

*  - Setting of the Local Bluetooth Device address from the host MCU

*

* On startup this demo:

*  - Initializes the Bluetooth sub system

*  - Receive NVRAM information from the host

*

* Application Instructions

*  - Connect a PC terminal to the serial port of the WICED Eval board.

*  - Start ClientControl application.

*  - Select the COM port assigned to the WICED Eval board.

*  - Download the application

*

* BR/EDR

* - To find BR/EDR devices: Click on "Start BR/EDR Discovery"

*

* Handsfree Connection

* - To create handsfree connection to remote AG device , choose the bluetooth

*   address of the remote AG device from the BR/EDR combo box

* - Click "Connect" button under Handsfree

* - OR Put the device in discoverable and connectable mode and serach for the device from AG device and connect

* - The following HF operations can be performed using the client control application

*      Connect / Disconnect HF or SCO connection

*      Answer / Hangup the call

*      Dial / Redial the number

*      Control Held call (ex. release all held calls, add held to conversion etc.)

*      Mic / Speaker gain control

View solution in original post

0 Likes
4 Replies
MiRo_263836
Level 5
Level 5
100 replies posted 50 likes received 50 replies posted

I was wrong;  The target is the CYW20706

0 Likes

Take a look at /20706-A2_Bluetooth/apps/snip/bt/hci_handsfree

* Features demonstrated

*  - WICED BT Handsfree (Device) APIs

*  - Handling of the UART WICED protocol

*  - SDP configuration

*  - Setting of the Local Bluetooth Device address from the host MCU

*

* On startup this demo:

*  - Initializes the Bluetooth sub system

*  - Receive NVRAM information from the host

*

* Application Instructions

*  - Connect a PC terminal to the serial port of the WICED Eval board.

*  - Start ClientControl application.

*  - Select the COM port assigned to the WICED Eval board.

*  - Download the application

*

* BR/EDR

* - To find BR/EDR devices: Click on "Start BR/EDR Discovery"

*

* Handsfree Connection

* - To create handsfree connection to remote AG device , choose the bluetooth

*   address of the remote AG device from the BR/EDR combo box

* - Click "Connect" button under Handsfree

* - OR Put the device in discoverable and connectable mode and serach for the device from AG device and connect

* - The following HF operations can be performed using the client control application

*      Connect / Disconnect HF or SCO connection

*      Answer / Hangup the call

*      Dial / Redial the number

*      Control Held call (ex. release all held calls, add held to conversion etc.)

*      Mic / Speaker gain control

0 Likes

Thank you. That looks like what I need.  Once I switched to the correct part in WICED, it cleared thing up.

0 Likes

No problem.  Note that HFP is not supported under the 20719.

0 Likes