Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

soG_4608441
Level 1
Level 1

Hi,

Is CYW920719 board supports USB interface.?

1 Solution

Discussion continued here: Need to send the hci commands to CYW920719 board with help of python libusb module. Which interface ...

20719 Supports HCI UART interface to send / receive HCI command . If you want a USB connection , then may need to connect USB to UART converter in between .

Thanks,

Anjana

View solution in original post

0 Likes
3 Replies
SheetalJ
Moderator
Moderator
Moderator
750 replies posted 500 likes received 500 replies posted

By USB interface, do you mean data transfer or interfacing another device over USB?

Please elaborate your query.

Hi Sheetal,

Thanks for reply.

I need to transfer the HCI commands over the USB interface from linux mahine. Is CYW920719 provides USB interface?. If it supports can I send HCI commands to the board using python pyusb module?

Regards,

Soumya Gadad

0 Likes

Discussion continued here: Need to send the hci commands to CYW920719 board with help of python libusb module. Which interface ...

20719 Supports HCI UART interface to send / receive HCI command . If you want a USB connection , then may need to connect USB to UART converter in between .

Thanks,

Anjana

0 Likes