- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Problem Overview:
We are trying to pair with IOS-13 beta and we support (HFP,A2DP,GATT,ANCS). So first Connect LE(GATT and ANCS) then Connect HFP but after sometime the HFP disconnects.
The Reason for the disconnection :
RCVD [0] Event from HCI. Name: HCI_Disconnection_Complete (Hex Code: 0x05 Param Len: 4)
Status : Success (0x00)
Connection Handle : 13 (0x000d)
Reason : 8 (0x08)
Connection Timeout
Observation1 : Based on the Attachment “bluetoothd-hci-latest_A2dp”
I see there was no response to the “AVDTP Discover” and there was disconnection which I think was initiated from the IOS-13. Please find the attachment and it also has IOS phone sniffer logs.
Observation2 : Based on Attachment “Handsfree_Disconnect_WithoutA2dp_IOS”
I disabled the A2DP from my code and re run the program but still there was a disconnection and there was same error but I think it was because, phone was not responding to AT+VGS and AT+VGM with Ok.
The log “Handsfree_Disconnect_WithoutA2dp_IOS”(Phone Log) and handsfree_disconnect_without_A2dp(Cypress log).
Note : We have also tried not to send AT+VGS after SLC connection but the behavior was still same.
Observation 3: Based on Attachment “handsfree_disconnect_3_withoutANCS”
I tried disabling the ANCS profile but still the disconnect was observed with same error.
Could you please help us to resolve this issues.
Note : “bluetoothd-hci-latest_a2dp.pklg” this is IOS log which can be opened in any MAC OS with PACKET logger.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi VaPa_4086226,
The BR/EDR disconnection events are due to a Link Timeout error (code 8). This error is typically a Baseband error (no packet received from the peer device).
I assume our team is working with you to resolve this problem, further updates will be provided via the technical case.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi VaPa_4086226,
The BR/EDR disconnection events are due to a Link Timeout error (code 8). This error is typically a Baseband error (no packet received from the peer device).
I assume our team is working with you to resolve this problem, further updates will be provided via the technical case.