Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

Hi,

could anybody help me with configuring the I2S/PCM interface when using A2DP source? (like in the watch demo)

Thanks,

Jeroen

1 Solution
AnjanaM_61
Moderator
Moderator
Moderator
First comment on KBA 5 questions asked First question asked

Hi Jeroen,

Q) We want to put the I2S/PCM interface in slave mode (MCU = master) and change the sample frequency according to our system configuration.

Ans:

In the watch example, we are setting to UART

static tAV_APP_CB av_app_cb;

av_app_cb.audio_route = AUDIO_ROUTE_UART ;

(Referring to watch app )

For setting to I2S,

set av_app_cb.audio_route = AUDIO_ROUTE_I2S ; 

Make sure while sending HCI_CONTROL_AUDIO_COMMAND_CONNECT you are setting route to I2S only

while calling wiced_audio_start function, set first argument to WICED_FALSE (mean is_master = WICED_FALSE)

 

you can set sampling frequency, while sending start you can update

or if you are already streaming you need to stop and start again with different freq.

av_app_cb.audio_sf = 'desired sampling frequency';

Could you please try the above settings?

Thanks & Regards,

Anjana

View solution in original post

6 Replies
AnjanaM_61
Moderator
Moderator
Moderator
First comment on KBA 5 questions asked First question asked

Hi Jeroen,

Could you please confirm which chip you are using? Also please clarify what exactly /which parameters you want to configure for I2S/PCM.

Thanks,
Anjana

0 Likes
Anonymous
Not applicable

Hi Anjana,

We are using the CW20706 (module CYBT-343026).

We want to put the I2C interface in slave mode (MCU = master) and change

the sample frequency b

0 Likes
Anonymous
Not applicable

(Sorry I pressed "send" by accident, my previous message was not complete

yet)

Hi Anjana,

We are using the CW20706 (module CYBT-343026).

We want to put the I2S/PCM interface in slave mode (MCU = master) and

change the sample frequency according to our system configuration.

We have 2 bluetooth modules on our product. If we configure the I2S/PCM

interface in the same way as we do on our other module (which has A2DP sink

and HFP functionality), the software crashes, even if we just try to read

it using "wiced_hal_get_pcm_config".

If you could tell us what the default settings are for the I2S/PCM

interface that would also be helpful.

Please treat this issue with highest priority because we are currently

blocked because of this issue.

Kind regards,

Jeroen

0 Likes
AnjanaM_61
Moderator
Moderator
Moderator
First comment on KBA 5 questions asked First question asked

Hi Jeroen,

Q) We want to put the I2S/PCM interface in slave mode (MCU = master) and change the sample frequency according to our system configuration.

Ans:

In the watch example, we are setting to UART

static tAV_APP_CB av_app_cb;

av_app_cb.audio_route = AUDIO_ROUTE_UART ;

(Referring to watch app )

For setting to I2S,

set av_app_cb.audio_route = AUDIO_ROUTE_I2S ; 

Make sure while sending HCI_CONTROL_AUDIO_COMMAND_CONNECT you are setting route to I2S only

while calling wiced_audio_start function, set first argument to WICED_FALSE (mean is_master = WICED_FALSE)

 

you can set sampling frequency, while sending start you can update

or if you are already streaming you need to stop and start again with different freq.

av_app_cb.audio_sf = 'desired sampling frequency';

Could you please try the above settings?

Thanks & Regards,

Anjana

Anonymous
Not applicable

Hello,

Which are the defaults pin to use for I2S? / How I can configure the I2S pin?

I tried to use I2S in master mode and configure the pin with the SuperMux GPIO Pin configuration but the pin stayed low.

Regards,

Thibaut.

0 Likes
Anonymous
Not applicable

Hi anpm

Is there any update on this? Could you give us some example code maybe

showing A2DP source with PCM/I2S?

Thanks,

Jeroen

0 Likes