- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi. I've read
which advices to write an empty app to the board. I've tried this
- Re: How to use standard HCI on CYW20819 / CYW920819EVB-02 Evaluation Kit?
explains to keep CTS high during reset.
I've connected the dev kit to my Mac and try examples of a third-party Bluetooth stack (btstack.org(.
If I press the Reset Button (SW2), and start the examples right away, I get this HCI sequence
- HCI Reset
- HCI Command Complete Event / Reset
- HCI Read Local Version Information
- HCI Command Complete Event / Local Version Information
- HCI Read Local Name
- HCI Hardware Error Event, HW Code 0x08
If I press the Reset Button, and wait 5 seconds, I get this
- HCI Reset
- HCI Hardware Error Event, HW Code 0x08
If I hold Recovery Button (SW1), then press Reset Button, I get this
- HCI Reset
- HCI Command Complete Event / Reset
- HCI Read Local Version Information
Nothing happens after this.
I've also seen Cypress Bluetooth SoC Programming Guide but I'm not sure how to get regular HCI to work.
If anybody wants to try, I'm using btstack/port/posix-h4 at master · bluekitchen/btstack · GitHub for testing.
Thanks!
Solved! Go to Solution.

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi ,
Not sure if your issue is resolved or not.
Whenever there is a full bluetooth application loaded, there will be HCI transaction going on from the application. The reason why its recommended to have an empty application is , it avoids any unwanted HCI transaction and will respond to the HCI commands sending from the host connected.
I had tested 20719 downloaded with empty application as suggested here: CYW20719 in HCI mode and was able to successfully communicate with CyBluetool several times.
Please make sure the CyBluetool settings are correct ( flow control enabled, HCI UART connected with baud rate 115200bps). Make sure HCI uart port is not connected to any other console when you try communicating with CyBluetool.
Thanks,
Anjana

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi ,
The method suggested in - CYW20719 in HCI mode should work for HCI commands testing.
Can you please try with our CyBluetool if you have a Windows or linux system CyBluetool (Linux Installer) CyBluetool (Windows Installer) ?
1. First please program from WICED SDK with an empty project with
#include "sparcommon.h"
APPLICATION_START() {}
and try sending commands with CyBluetool.
Thanks,
Anjana

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
I've put the suggested code into a file hci.c:
#include "sparcommon.h"
APPLICATION_START() {}
and have a Makefile with
NAME := hci
APP_SRC = hci.c
then, I've uploaded it with
$ ./make snip.bt.hci-CYW920719Q40EVB_01 download
Compiling spar_setup.c
Compiling hci.c
Compiling wiced_platform.c
Compiling wiced_platform_pin_config.c
Compiling lib_installer.c
Linking target ELF
OK, made elf.
../../43xxx_Wi-Fi/tools/ARM_GNU/OSX/bin/arm-none-eabi-objdump: section '.ordered' mentioned in a -j option, but not found in any input file
../../43xxx_Wi-Fi/tools/ARM_GNU/OSX/bin/arm-none-eabi-objdump: section '.data' mentioned in a -j option, but not found in any input file
../../43xxx_Wi-Fi/tools/ARM_GNU/OSX/bin/arm-none-eabi-objdump: section '.aon' mentioned in a -j option, but not found in any input file
../../43xxx_Wi-Fi/tools/ARM_GNU/OSX/bin/arm-none-eabi-objdump: section '.pram_rodata' mentioned in a -j option, but not found in any input file
Call to hci_spar_crt_setup @ 00215871
OK, made /Projects/Broadcom/WICED-Studio-6.2.1-SDK/20719-B1_Bluetooth/WICED/../build/hci-CYW920719Q40EVB_01-rom-ram-Wiced-release/A_20719B1-hci-rom-ram-spar.cgs. MD5 sum is:
51b74b98f13dbe141f0396550673a97c ../build/hci-CYW920719Q40EVB_01-rom-ram-Wiced-release/A_20719B1-hci-rom-ram-spar.cgs
--------------------------------------------------------------------------------
Patch code starts at 0x00270400 (RAM address)
Patch code ends at 0x0027ACD8 (RAM address)
Patch RW/ZI size 2936 bytes
Application starts at 0x00215768 (RAM address)
Application ends at 0x00215870 (RAM address)
Patch code size 43224 bytes
Application RAM footprint 264 bytes
------
Total RAM footprint 3200 bytes (3.1kiB)
--------------------------------------------------------------------------------
Converting CGS to HEX...
Conversion complete
Creating OTA images...
Conversion complete
OTA image footprint in NV is 50218 bytes
Detecting device...
Device found
Downloading application...
Download complete
Application running.
Now. I start CyBluetool on Windows and connect to the controller successfully.
07/11/19 13:50:36.452 com2 -- Transport opened
com2@115200
07/11/19 13:50:36.452 com2 -- Protocol set to HCI
com2@115200
Then, I execute an HCI Reset
07/11/19 13:51:22.788 com2@115200 c> Reset
HCI Command
com2@115200
[03 0C 00 ]
opcode = 0x0C03 (3075, "Reset")
07/11/19 13:51:22.803 com2 <e Hardware Error
HCI Event
com2@115200
[10 01 ]: 00
event = 0x10 (16,"Hardware Error")
Hardware_Code = 0x0 (0, "UART Parsing Error")
07/11/19 13:51:22.834 com2 <e Vendor Specific
HCI Event
com2@115200
[FF 08 ]: 1B 04 01 00 00 79 01 00
event = 0xFF (255,"Vendor Specific")
Event_Sub_Code = 0x1B (27, "DBFW Dump")
Dump Type = 0x4 (4, "DBFW TraceDump2")
Nof T = 0x1 (1)
Trace Status = 0x0 (0, "")
TRACE-1 = "00 79 01 00"
I did not expect to get the Hardware error. What did I do wrong?

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
After successfully following the Run CYW20706 in HCI Modeguide with the 20706 dev kit, I've tried the same approach with the 20719: disabled the trace log by wiced_set_debug_uart(WICED_ROUTE_DEBUG_NONE) in the hello_sensor demo application and keep CTS high during RESET - the USB UART is closed when pressing RESET button.
With this, the 20719 is mostly working over HCI. Could somebody explain the difference between an empty application and a full Bluetooth application? Is this correct?
During startup, I get a few 'HCI Event Command Complete - Command Disallowed" for HCI Reset, HCI Read Local Name, HCI Set Event Mask, ... more or less all configuration commands. Any ideas about this?

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi ,
Not sure if your issue is resolved or not.
Whenever there is a full bluetooth application loaded, there will be HCI transaction going on from the application. The reason why its recommended to have an empty application is , it avoids any unwanted HCI transaction and will respond to the HCI commands sending from the host connected.
I had tested 20719 downloaded with empty application as suggested here: CYW20719 in HCI mode and was able to successfully communicate with CyBluetool several times.
Please make sure the CyBluetool settings are correct ( flow control enabled, HCI UART connected with baud rate 115200bps). Make sure HCI uart port is not connected to any other console when you try communicating with CyBluetool.
Thanks,
Anjana