How to use standard HCI on CYW20719 / CYW920719Q40EVB-01 Evaluation Kit?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
mringwal
Level 4
Level 4
Associated Partner - BlueKitchen GmbH
5 sign-ins 10 questions asked 10 replies posted

Hi. I've read

- CYW20719 in HCI mode

which advices to write an empty app to the board. I've tried this

- Re: How to use standard HCI on CYW20819 / CYW920819EVB-02 Evaluation Kit?

explains to keep CTS high during reset.

I've connected the dev kit to my Mac and try examples of a third-party Bluetooth stack (btstack.org(.

If I press the Reset Button (SW2), and start the examples right away, I get this HCI sequence

- HCI Reset

- HCI Command Complete Event / Reset

- HCI Read Local Version Information

- HCI Command Complete Event / Local Version Information

- HCI Read Local  Name

- HCI Hardware Error Event, HW Code 0x08

If I press the Reset Button, and wait 5 seconds, I get this

- HCI Reset

- HCI Hardware Error Event, HW Code 0x08

If I hold Recovery Button (SW1), then press Reset Button, I get this

- HCI Reset

- HCI Command Complete Event / Reset

- HCI Read Local Version Information

Nothing happens after this.

I've also seen Cypress Bluetooth SoC Programming Guide​ but I'm not sure how to get regular HCI to work.

If anybody wants to try, I'm using btstack/port/posix-h4 at master · bluekitchen/btstack · GitHub for testing.

Thanks!

0 Likes
1 Solution
AnjanaM_61
Moderator
Moderator
Moderator
10 questions asked 5 comments on KBA First comment on KBA

Hi ,

Not sure if your issue is resolved or not.

Whenever there is a full bluetooth application loaded, there will be HCI transaction going on from the application. The reason why its recommended to have an empty application is , it avoids any unwanted HCI transaction and will respond to the HCI commands sending from the host connected.

I had tested 20719 downloaded with empty application as suggested here: CYW20719 in HCI mode  and was able to successfully communicate with CyBluetool several times.

Please make sure the CyBluetool settings are correct ( flow control enabled, HCI UART connected with baud rate 115200bps). Make sure HCI uart port is not connected to any other console when you try communicating with CyBluetool.

Thanks,
Anjana

View solution in original post

4 Replies
AnjanaM_61
Moderator
Moderator
Moderator
10 questions asked 5 comments on KBA First comment on KBA

Hi ,

The method suggested in - CYW20719 in HCI mode should work for HCI commands testing.

Can you please try with our CyBluetool if you have a Windows or linux system CyBluetool (Linux Installer) CyBluetool (Windows Installer)  ?

1. First please program from WICED SDK with an empty project with

#include "sparcommon.h"

APPLICATION_START() {}

and try sending commands with CyBluetool.

Thanks,

Anjana

mringwal
Level 4
Level 4
Associated Partner - BlueKitchen GmbH
5 sign-ins 10 questions asked 10 replies posted

I've put the suggested code into a file hci.c:

#include "sparcommon.h"

APPLICATION_START() {}

and have a Makefile with

NAME := hci

APP_SRC  = hci.c

then, I've uploaded it with

$ ./make snip.bt.hci-CYW920719Q40EVB_01 download

Compiling spar_setup.c

Compiling hci.c

Compiling wiced_platform.c

Compiling wiced_platform_pin_config.c

Compiling lib_installer.c

Linking target ELF

OK, made elf.

../../43xxx_Wi-Fi/tools/ARM_GNU/OSX/bin/arm-none-eabi-objdump: section '.ordered' mentioned in a -j option, but not found in any input file

../../43xxx_Wi-Fi/tools/ARM_GNU/OSX/bin/arm-none-eabi-objdump: section '.data' mentioned in a -j option, but not found in any input file

../../43xxx_Wi-Fi/tools/ARM_GNU/OSX/bin/arm-none-eabi-objdump: section '.aon' mentioned in a -j option, but not found in any input file

../../43xxx_Wi-Fi/tools/ARM_GNU/OSX/bin/arm-none-eabi-objdump: section '.pram_rodata' mentioned in a -j option, but not found in any input file

Call to hci_spar_crt_setup @ 00215871

OK, made /Projects/Broadcom/WICED-Studio-6.2.1-SDK/20719-B1_Bluetooth/WICED/../build/hci-CYW920719Q40EVB_01-rom-ram-Wiced-release/A_20719B1-hci-rom-ram-spar.cgs. MD5 sum is:

51b74b98f13dbe141f0396550673a97c ../build/hci-CYW920719Q40EVB_01-rom-ram-Wiced-release/A_20719B1-hci-rom-ram-spar.cgs

--------------------------------------------------------------------------------

Patch code starts at              0x00270400 (RAM address)

Patch code ends at                0x0027ACD8 (RAM address)

Patch RW/ZI size                  2936 bytes

Application starts at             0x00215768 (RAM address)

Application ends at               0x00215870 (RAM address)

Patch code size                        43224 bytes

Application RAM footprint                264 bytes

                                      ------

Total RAM footprint                     3200 bytes (3.1kiB)

--------------------------------------------------------------------------------

Converting CGS to HEX...

Conversion complete

Creating OTA images...

Conversion complete

OTA image footprint in NV is 50218 bytes

Detecting device...

Device found

Downloading application...

Download complete

Application running.

Now. I start CyBluetool on Windows and connect to the controller successfully.

07/11/19 13:50:36.452 com2 -- Transport opened

com2@115200

07/11/19 13:50:36.452 com2 -- Protocol set to HCI

com2@115200

Then, I execute an HCI Reset

07/11/19 13:51:22.788 com2@115200 c> Reset

HCI Command

com2@115200

[03 0C 00 ]

opcode = 0x0C03 (3075, "Reset")

07/11/19 13:51:22.803 com2 <e Hardware Error

HCI Event

com2@115200

[10 01 ]: 00

event = 0x10 (16,"Hardware Error")

Hardware_Code = 0x0 (0, "UART Parsing Error")

07/11/19 13:51:22.834 com2 <e Vendor Specific

HCI Event

com2@115200

[FF 08 ]: 1B 04 01 00 00 79 01 00

event = 0xFF (255,"Vendor Specific")

Event_Sub_Code = 0x1B (27, "DBFW Dump")

Dump Type = 0x4 (4, "DBFW TraceDump2")

Nof T = 0x1 (1)

Trace Status = 0x0 (0, "")

TRACE-1 = "00 79 01 00"

I did not expect to get the Hardware error. What did I do wrong?

0 Likes
mringwal
Level 4
Level 4
Associated Partner - BlueKitchen GmbH
5 sign-ins 10 questions asked 10 replies posted

After successfully following the Run CYW20706 in HCI Mode​guide with the 20706 dev kit, I've tried the same approach with the 20719: disabled the trace log by wiced_set_debug_uart(WICED_ROUTE_DEBUG_NONE) in the hello_sensor demo application and keep CTS high during RESET - the USB UART is closed when pressing RESET button.

With this, the 20719 is mostly working over HCI. Could somebody explain the difference between an empty application and a full Bluetooth application? Is this correct?

During startup, I get a few 'HCI Event Command Complete - Command Disallowed" for HCI Reset, HCI Read Local Name, HCI Set Event Mask, ... more or less all configuration commands. Any ideas about this?

0 Likes
AnjanaM_61
Moderator
Moderator
Moderator
10 questions asked 5 comments on KBA First comment on KBA

Hi ,

Not sure if your issue is resolved or not.

Whenever there is a full bluetooth application loaded, there will be HCI transaction going on from the application. The reason why its recommended to have an empty application is , it avoids any unwanted HCI transaction and will respond to the HCI commands sending from the host connected.

I had tested 20719 downloaded with empty application as suggested here: CYW20719 in HCI mode  and was able to successfully communicate with CyBluetool several times.

Please make sure the CyBluetool settings are correct ( flow control enabled, HCI UART connected with baud rate 115200bps). Make sure HCI uart port is not connected to any other console when you try communicating with CyBluetool.

Thanks,
Anjana