Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

ns_4270701
Level 3
Level 3
10 replies posted 10 questions asked 5 replies posted

Development environment:

Windows 8.1 pro

Platform: CYBT-423028-02

IDE: Wiced Studio 6.2.1

Just as an example :

Created service A

    It has 2 characteristics  B and C

B characteristic has Read and Write property n permission

characteristic has Read and Notify property n permission

We have developed a demo code and created a characteristic(C) of one of the services(A) with "Notify" property.

Once the peer device writes into the client configuration of (C), I  get the 0x1000 for notification.

But when we use the same characteristic to send the notification value, A peer device is not getting any notification. Please tell me which attr handle should be used to send the notification to peer device, please share the example.

wiced_bt_gatt_status_t wiced_bt_gatt_send_notification (uint16_t conn_id, uint16_t attr_handle, uint16_t val_len, uint8_t *p_val );

conn_id                 = connected device's id

attr_handle         = (Characteristic C )CLIENT_CONFIGURATION , handle

val_len                  = length of the actual data to be shared with a connected device

p_val                     = Notification value

Please note we have followed the steps from the "demo.sensor" project, but it doesn't work in our code.

So please provide me the proper example of it.

0 Likes
1 Solution

Found the issue.. the connection ID was updated wrong..  Thanks anyways.

View solution in original post

0 Likes
4 Replies
DheerajPK_41
Moderator
Moderator
Moderator
750 replies posted 500 likes received 500 replies posted

Hi,

You need to use Characteristic value handle from the gatt_db_lookup_table_t. Could you please check below lab manual program to understand the usage of wiced_bt_gatt_send_notification.

CypressAcademy_WBT101_Files/Projects/ch04b/key_ch04b_ex01_ctr at master · cypresssemiconductorco/Cyp...

If you can attach your relevant code snippet and Gatt DB config, we can give you more specific suggestions.

Thanks,

-Dheeraj

Please see the generated files below using wiced ble designer...

And we could not find any notification value handle,  as we can see in demo.sensor code.

// *********************************************************************************************************************************

//********************************************************testnotifynuart_db.c***************************************************

// *********************************************************************************************************************************

#include "wiced_bt_uuid.h"

#include "wiced_bt_gatt.h"

#include "testnotifynuart_db.h"

/*************************************************************************************

** GATT server definitions

*************************************************************************************/

const uint8_t gatt_database[] = // Define GATT database

{

    /* Primary Service 'Generic Attribute' */

    PRIMARY_SERVICE_UUID16 (HDLS_GENERIC_ATTRIBUTE, UUID_SERVICE_GATT),

    /* Primary Service 'Generic Access' */

    PRIMARY_SERVICE_UUID16 (HDLS_GENERIC_ACCESS, UUID_SERVICE_GAP),

        /* Characteristic 'Device Name' */

        CHARACTERISTIC_UUID16 (HDLC_GENERIC_ACCESS_DEVICE_NAME, HDLC_GENERIC_ACCESS_DEVICE_NAME_VALUE,

            UUID_CHARACTERISTIC_DEVICE_NAME, LEGATTDB_CHAR_PROP_READ,

            LEGATTDB_PERM_READABLE),

        /* Characteristic 'Appearance' */

        CHARACTERISTIC_UUID16 (HDLC_GENERIC_ACCESS_APPEARANCE, HDLC_GENERIC_ACCESS_APPEARANCE_VALUE,

            UUID_CHARACTERISTIC_APPEARANCE, LEGATTDB_CHAR_PROP_READ,

            LEGATTDB_PERM_READABLE),

    /* Primary Service 'testnotifynuartServc' */

    PRIMARY_SERVICE_UUID128 (HDLS_TESTNOTIFYNUARTSERVC, __UUID_TESTNOTIFYNUARTSERVC),

        /* Characteristic 'testnotifynuartChar' */

        CHARACTERISTIC_UUID128 (HDLC_TESTNOTIFYNUARTSERVC_TESTNOTIFYNUARTCHAR, HDLC_TESTNOTIFYNUARTSERVC_TESTNOTIFYNUARTCHAR_VALUE,

            __UUID_TESTNOTIFYNUARTSERVC_TESTNOTIFYNUARTCHAR, LEGATTDB_CHAR_PROP_NOTIFY,

            LEGATTDB_PERM_NONE),

            /* Descriptor 'Characteristic User Description' */

            CHAR_DESCRIPTOR_UUID16 (HDLD_TESTNOTIFYNUARTSERVC_TESTNOTIFYNUARTCHAR_USER_DESCRIPTION,

                UUID_DESCRIPTOR_CHARACTERISTIC_USER_DESCRIPTION, LEGATTDB_PERM_READABLE),

            /* Descriptor 'Client Characteristic Configuration' */

            CHAR_DESCRIPTOR_UUID16_WRITABLE (HDLD_TESTNOTIFYNUARTSERVC_TESTNOTIFYNUARTCHAR_CLIENT_CONFIGURATION,

                UUID_DESCRIPTOR_CLIENT_CHARACTERISTIC_CONFIGURATION, LEGATTDB_PERM_READABLE | LEGATTDB_PERM_WRITE_REQ | LEGATTDB_PERM_AUTH_WRITABLE),

};

// Length of the GATT database

const uint16_t gatt_database_len = sizeof(gatt_database);

// ***************************************************************************************************************************************************************

// ************************************************************ testnotifynuart_db.h ***************************************************************************

// ***************************************************************************************************************************************************************

#ifndef __GATT_DATABASE_H__

#define __GATT_DATABASE_H__

#define __UUID_TESTNOTIFYNUARTSERVC                                        0xfc, 0xf9, 0xb4, 0x7e, 0xf4, 0x9d, 0x4f, 0x18, 0xbd, 0x79, 0x3a, 0xf5, 0xdd, 0x12, 0xf0, 0xce

#define __UUID_TESTNOTIFYNUARTSERVC_TESTNOTIFYNUARTCHAR                    0xf9, 0x41, 0x1a, 0xb0, 0x9f, 0x73, 0x4b, 0x97, 0xb5, 0x2f, 0x84, 0x48, 0x8a, 0x27, 0xc2, 0x73

// ***** Primary Service 'Generic Attribute'

#define HDLS_GENERIC_ATTRIBUTE                                             0x0001

// ***** Primary Service 'Generic Access'

#define HDLS_GENERIC_ACCESS                                                0x0014

// ----- Characteristic 'Device Name'

#define HDLC_GENERIC_ACCESS_DEVICE_NAME                                    0x0015

#define HDLC_GENERIC_ACCESS_DEVICE_NAME_VALUE                              0x0016

// ----- Characteristic 'Appearance'

#define HDLC_GENERIC_ACCESS_APPEARANCE                                     0x0017

#define HDLC_GENERIC_ACCESS_APPEARANCE_VALUE                               0x0018

// ***** Primary Service 'testnotifynuartServc'

#define HDLS_TESTNOTIFYNUARTSERVC                                          0x0028

// ----- Characteristic 'testnotifynuartChar'

#define HDLC_TESTNOTIFYNUARTSERVC_TESTNOTIFYNUARTCHAR                      0x0029

#define HDLC_TESTNOTIFYNUARTSERVC_TESTNOTIFYNUARTCHAR_VALUE                0x002A

// ===== Descriptor 'User Description'

#define HDLD_TESTNOTIFYNUARTSERVC_TESTNOTIFYNUARTCHAR_USER_DESCRIPTION     0x002B

// ===== Descriptor 'Client Configuration'

#define HDLD_TESTNOTIFYNUARTSERVC_TESTNOTIFYNUARTCHAR_CLIENT_CONFIGURATION 0x002C

// External Lookup Table Entry

typedef struct

{

    uint16_t handle;

    uint16_t max_len;

    uint16_t cur_len;

    uint8_t  *p_data;

} gatt_db_lookup_table;

// External definitions

extern const uint8_t  gatt_database[];

extern const uint16_t gatt_database_len;

extern gatt_db_lookup_table testnotifynuart_gatt_db_ext_attr_tbl[];

extern const uint16_t testnotifynuart_gatt_db_ext_attr_tbl_size;

extern uint8_t BT_LOCAL_NAME[];

extern const uint16_t BT_LOCAL_NAME_CAPACITY;

#endif /* __GATT_DATABASE_H__ */

0 Likes
AnjanaM_61
Moderator
Moderator
Moderator
First comment on KBA 5 questions asked First question asked

Hi ns_4270701 ,

As DheerajP_41 mentioned, please provide us code to check at our side.

What is the peer device you are using ?

Did you check the return value of wiced_bt_gatt_send_notification function ?

Regards,

Anjana

0 Likes

Found the issue.. the connection ID was updated wrong..  Thanks anyways.

0 Likes