Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

NAYU_1212731
Level 1
First like given
Level 1

Hi, I am currently connecting to CYW20706 with our MPU.

I sent the HCI_RESER command"01 03 0C 00" to CYW20706 from MPU.

And I got the HCI command"04 13 05 01 0B 00 01 00 04 0E 04 01 03 0C" from CYW20706.

I know the "04 0E 04 01 03 0C" meaning, but I don't know "04 13 05 01 0B 00 01 00".

Could you tell this command "04 13 05 01 0B 00 01 00" meaning?  

Thank you!

Best regards,

Yuji

0 Likes
1 Solution
MuraliR_36
Moderator
Moderator 250 sign-ins 250 replies posted 100 solutions authored
Moderator

Hi Yuji,

I would guess that the chip is transmitting NVRAM data which can be inferred form the initial byte 04 that is being received.

Also 04 indicates that multiple chunks of non contiguous NVRAM data may be received.

If you look into the WICED-HCI-CONTROL-PROTOCOL.pdf found in the docs of 20706 in WICED studio, the following could be inferred

04-> NVRAM Data

Next 2 bytes->NVRAM ID

Next 2 bytes-> NVRAM Data

The Next 00 indicates that it is the end of that block of data.

The Following 01 indicates the command status and the 00 which follows indicates that the execution has started.

The data received after this is the acknowledgement for the HCI_RESET command.

Try putting the device into recovery mode and then sending the command. You should get the proper HCI reset response.

Thanks

View solution in original post

2 Replies
BoonT_56
Employee
500 likes received 250 likes received 100 likes received
Employee

I'm not sure what this string of tuples mean, but the last byte 0x0C refers to "Command Disallowed" according to the list of error codes.

0 Likes
MuraliR_36
Moderator
Moderator 250 sign-ins 250 replies posted 100 solutions authored
Moderator

Hi Yuji,

I would guess that the chip is transmitting NVRAM data which can be inferred form the initial byte 04 that is being received.

Also 04 indicates that multiple chunks of non contiguous NVRAM data may be received.

If you look into the WICED-HCI-CONTROL-PROTOCOL.pdf found in the docs of 20706 in WICED studio, the following could be inferred

04-> NVRAM Data

Next 2 bytes->NVRAM ID

Next 2 bytes-> NVRAM Data

The Next 00 indicates that it is the end of that block of data.

The Following 01 indicates the command status and the 00 which follows indicates that the execution has started.

The data received after this is the acknowledgement for the HCI_RESET command.

Try putting the device into recovery mode and then sending the command. You should get the proper HCI reset response.

Thanks