- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Team,
I'm working with a customer using the 20719 within an application that is extremely sensitive errors and re-transmission.
Per the blog RanjithK_41 created here: CYW20719 and CYW20735 Peripheral and HCI UARTs
The PUART on the 20719 will operate up to 3Mb/s max. However, they want to understand whether or not there is an associated error rate which needs to be calculated in order to assess actual throughput and potential for re-transmission of data.
As an example, the STM32 MCU documents a 1.73% error rate on its 3Mb/s UART, so they want to understand if our UART implementation is similar.
Thanks in advance for your help.
Solved! Go to Solution.
- Tags:
- error rate puart
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
In the 20706 datasheet, there is a chart (Table 2) displaying the error rates for the various baud rates. I noted that this chart was absent in the 20719 datasheet. There is another statement saying that if the combined baud rate error of the device and host is within +/- 5%, then the device (20719) operates correctly. Is this what you are looking for?