Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

KeTa_1341526
Level 5
Level 5
5 likes given First like given 10 solutions authored

Hello,

In the following Community, it is described in MTU Size of PSoC BLE version.

Re: How to change MTU size for EZ-Serial BLE

Similarly, what is the MTU Size allowed by the EZ-Serial Firmware of the CYW2070 x-based Module (CYBT-343026)?

Best regards,

Takahashi

0 Likes
1 Solution

Are you using the EZ-Serial FW?

If yes, please refer to the following user guide in chapter 7.2.8.4: EZ-Serial WICED Firmware Platform User Guide for CYW2070x-based Modules (cypress.com)

View solution in original post

0 Likes
3 Replies
Owen_Zhang123
Moderator
Moderator
Moderator
500 solutions authored 250 sign-ins 1000 replies posted

The maximum MTU size for the CYW2070x-based module is 512 bytes.

0 Likes

Thank you for your response.

As a confirmation, I think the UART receive buffer is 128 bytes.

Please tell me about the case where MTU size of 128Byte (MTU Size is 131byte = Header: 3byte + Data: 128Byte) or more is requested by Central.

In this case, does the BT Stack start Notify transmission when the specified MTU size of data is sent from the Host MCU?

Best regards,

Takahashi

0 Likes

Are you using the EZ-Serial FW?

If yes, please refer to the following user guide in chapter 7.2.8.4: EZ-Serial WICED Firmware Platform User Guide for CYW2070x-based Modules (cypress.com)

0 Likes