Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

JoJo_2624151
Level 3
Level 3
First like received First like given

     Two switches on AAC are found in SDK.

     Are there any differences between the two?

微信截图_20180402135805.png

0 Likes
1 Solution
Anonymous
Not applicable

Firstly, the AAC codec library is not available with WICED 6.1. In the makefile, A2DP_EXT_CODED is forced to 0 because the current SDK does not have a library for AAC.

View solution in original post

4 Replies
Anonymous
Not applicable

Firstly, the AAC codec library is not available with WICED 6.1. In the makefile, A2DP_EXT_CODED is forced to 0 because the current SDK does not have a library for AAC.

Is there a plan to add

0 Likes
Anonymous
Not applicable

There is a plan but it is too early to post a 'definite yes' as of now.

0 Likes

Hi yssu:

          thank you!

0 Likes