- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Cyw20706 Systick's smallest minimum timer resolution is 12.5ms???Include/wiced_Timer.h Line 52 "Defines the wiced timer types. These timers are system tick driven and a systick is 12.5 milliseconds.So the minimum timer resolution supported is 12.5 milliseconds"
If not, how to set it smaller?
/*
* Defines the wiced timer types. These timers are system tick driven and a
* systick is 12.5 milliseconds.So the supported is
* 12.5 milliseconds
*/
typedef enum
{
WICED_SECONDS_TIMER = 1,
WICED_MILLI_SECONDS_TIMER, /* The minimum resolution supported is 12.5 ms */
WICED_SECONDS_PERIODIC_TIMER,
WICED_MILLI_SECONDS_PERIODIC_TIMER /*The minimum resolution supported is 12.5 ms */
}wiced_timer_type_t;
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi tanggh_2945091,
CYW20706 is an old chip and the firmware in its ROM is also old. It can give only 12ms minimum timer resolution. There is no way to reduce this value further.
Other Bluetooth chips like CYW20735, CYW20719 can give upto 1ms minimum resolution.