- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I'm following the instructions in the CyBluetool User guide for activating the transmit tests. Even though the device under test (DUT) returns "success" to the commands, there is no corresponding spike on the spectrum analyzer when following the instructions in the user guide. Can you please explain how to get this command to work?
The user guide walks through using Set_Tx_CarrierFrequency_ARM at 2402 MHz. In the following trace you can see that this is successful
10/28/19 08:42:27.502 com35 c> Set_Tx_Carrier_Frequency_ARM
HCI Command
com35@115200
[14 FC 07 ]: 00 02 01 00 00 00 00
opcode = 0xFC14 (64532, "Set_Tx_Carrier_Frequency_ARM")
Carrier_Enable = 0x0 (0, "Carrier on")
Carrier_Frequency_Encoded = 0x2 (2)
Carrier_Frequency = 0x962 (2402, MHz)
Mode = 0x1 (1, "PRBS9")
Modulation Type = 0x0 (0, "GFSK")
Transmit_Power = 0x0 (0, "0 dBm")
Transmit_Power_dBm = 0x0 (0, dBm)
Transmit_Power_Table_Index = 0x0 (0)
10/28/19 08:42:27.508 com35 <c Set_Tx_Carrier_Frequency_ARM
HCI Command Complete Event
com35@115200
[0E 04 ]: 01 14 FC 00
event = 0x0E (14,"Command Complete")
Num_HCI_Command_Packets = 0x1 (1)
Command_Opcode = 0xFC14 (64532, "Set_Tx_Carrier_Frequency_ARM")
Status = 0x0 (0, "Success", "Success")
But the spectrum analyzer shows no spike at 2402MHz
When I send a LE_Transmitter_Test_[v2] at 2402MHz, I do get the expected result
10/28/19 08:40:20.205 com35 <c LE_Transmitter_Test_[v2]
HCI Command Complete Event
com35@115200
[0E 04 ]: 01 34 20 00
event = 0x0E (14,"Command Complete")
Num_HCI_Command_Packets = 0x1 (1)
Command_Opcode = 0x2034 (8244, "LE_Transmitter_Test_[v2]")
Status = 0x0 (0, "Success", "Success")
10/28/19 08:42:01.804 com35 c> Set_Tx_Carrier_Frequency_ARM
HCI Command
com35@115200
[14 FC 07 ]: 00 02 01 00 00 00 00
opcode = 0xFC14 (64532, "Set_Tx_Carrier_Frequency_ARM")
Carrier_Enable = 0x0 (0, "Carrier on")
Carrier_Frequency_Encoded = 0x2 (2)
Carrier_Frequency = 0x962 (2402, MHz)
Mode = 0x1 (1, "PRBS9")
Modulation Type = 0x0 (0, "GFSK")
Transmit_Power = 0x0 (0, "0 dBm")
Transmit_Power_dBm = 0x0 (0, dBm)
Transmit_Power_Table_Index = 0x0 (0)
You'll see that with the LE_Transmitter_Test_[v2] command we do see a spike at 2402MHz as expected.
Can you please explain how to get the Set_Tx_CarrierFrequency_ARM to work as shown in the user guide?
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I was unable to reproduce the problem today, everything worked well. I think, perhaps, yesterday I had forgotten to load a non-bluetooth project into the module before starting CyBlueTool. Today I built and downloaded the snip.hal.gpio project first, perhaps I didn't yesterday. Sorry to have bothered you.