Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

lock attach
Attachments are accessible only for community members.
KaLa_4346091
Level 1
Level 1
5 likes given First like received First like given

hello,

          I am a student working on the kit CYW920819 EVB-02. Recently, when I was working with the kit, the carrier module present on the board got separated from the board(I guess it would have happened when I was taking it to my home) as shown in the enclosed attachments. Then I tested it by dumping the example codes such as FindMe profile. But as expected, the serial port was not being detected and the download is being failed. (although the led blinks during detection, the supply is being given)

Is there any chance of making the kit work by soldering the module to the board (If so, How?) or should I get a new one? Please suggest a way for the kit to work...

1 Solution
1 Reply
AnjanaM_61
Moderator
Moderator
Moderator
First comment on KBA 5 questions asked First question asked

Discussion is going on in duplicate thread here :Carrier Module broken: Hardware Damaged in CYW920819 EVB-02 BLE Board

0 Likes