Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth

phwh_4072786
Level 2
First like received
Level 2

Downloading demos to my CYW920719Q40EVB-01 is very inconsistent. It fails a majority of the time. If the UART port is not explicitly set, it cannot find the device. If I set the UART in the target, I get the error:

15:02:08 **** Build of configuration Release for project 20719-B1_Bluetooth ****

"F:\\Packages\\WICED-Studio-6.2\\20719-B1_Bluetooth\\make.exe" wiced_bt_class.L3_SuperMux-CYW920719Q40EVB_01 download UART=COM9

Linking target ELF

OK, made elf.

..\..\43xxx_Wi-Fi\tools\ARM_GNU\Win32\bin\arm-none-eabi-objdump: section '.ordered' mentioned in a -j option, but not found in any input file

..\..\43xxx_Wi-Fi\tools\ARM_GNU\Win32\bin\arm-none-eabi-objdump: section '.aon' mentioned in a -j option, but not found in any input file

..\..\43xxx_Wi-Fi\tools\ARM_GNU\Win32\bin\arm-none-eabi-objdump: section '.pram_rodata' mentioned in a -j option, but not found in any input file

Call to L3_SuperMux_spar_crt_setup @ 002159d9

OK, made F:/Packages/WICED-Studio-6.2/20719-B1_Bluetooth/WICED/../build/L3_SuperMux-CYW920719Q40EVB_01-rom-ram-Wiced-release/A_20719B1-L3_SuperMux-rom-ram-spar.cgs. MD5 sum is:

6e82d92b536a9a624a4d5c728ba16f6b *../build/L3_SuperMux-CYW920719Q40EVB_01-rom-ram-Wiced-release/A_20719B1-L3_SuperMux-rom-ram-spar.cgs

--------------------------------------------------------------------------------

Patch code starts at              0x00270400 (RAM address)

Patch code ends at                0x0027ACD8 (RAM address)

Patch RW/ZI size                  2936 bytes

Application starts at             0x00215768 (RAM address)

Application ends at               0x002159D8 (RAM address)

Patch code size                        43224 bytes

Application RAM footprint                624 bytes

                                      ------

Total RAM footprint                     3560 bytes (3.5kiB)

--------------------------------------------------------------------------------

Converting CGS to HEX...

Conversion complete

Creating OTA images...

Conversion complete

OTA image footprint in NV is 50584 bytes

Downloading application...

****Download failed ****

Trying baudrate 115200   Conn: PORT=COM9    BAUDRATE=115200

Trying baudrate 3000000   Conn: PORT=COM9    BAUDRATE=3000000

Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%).   Current state: Terminated with error

Failed to determine baud rate

Download failed. This WICED platform of the SDK only supports download to 207x9B1 devices.

Follow the instructions in the 20719-B1 README.txt for downloading the application.

15:02:23 Build Finished (took 14s.756ms)

Hitting reset or doing a recover (-> Sw1 -> Sw2 <- Sw2 <- Sw1) does not fix the problem.

0 Likes
1 Solution
phwh_4072786
Level 2
First like received
Level 2

It seems that the board came broken. Uploading projects to other boards works fine. Specifically, the recover function on the original board does not work. It keeps running the prior program after recovery and does not accept new ones.

View solution in original post

3 Replies